SPRADC4 june 2023 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1
In a camera mirror system, the image data from the camera typically goes through the CSI-2 RX interface, ISP, deep learning engine, and finally to the display. Figure 5-1shows the data flow on the AM62A device.
For camera mirror applications, the latency from camera to display (that is, the so-called glass-to-glass latency) must be as small as possible. Every block in the data flow contributes to the latency. The AM62A SoC has the following differentiating features that can achieve optimal latency:
Table 5-1 shows an exemplary analysis of the latency accumulated block after block in the data path shown in Figure 5-1. A 2.1MP (1936 × 1100) sensor running at 60 fps is used for the analysis. The latency introduced by each block is estimated as the following:
| Sensor 1936 × 1100 at 60 fps | Frame 0 | ||||||
| CSI2-RX | Frame 0 | ||||||
| VISS | Frame 0 | ||||||
| LDC | Frame 0 | ||||||
| MSC | Frame 0 | ||||||
| Deep Learning | Frame 0 | ||||||
| Display | Frame 0 | ||||||
| Time (ms) | 0 | 16.67 | 24.67 | 32.67 | 40.67 | 48.67 | 65.33 |
As shown in this analysis, the total latency of the data flow shown in Figure 5-1 is about 65ms, which is adequate for a typical camera mirror system.