SPRADE8A November 2023 – April 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Single-Unit Emulation is similar to the Ping Pong Emulation, but only uses one set of Flash Sectors. Thus, the Ping Pong method cannot be used and when a full EEPROM is detected. The implemented behavior is shown in this section. Many of the functions remain the same between the two modes, and the primary differences are seen in the Erase behavior.