SPRT843 October   2026 TLV709 , TPS7A16A , TPS7A24 , TPS7A26 , TPS7A43 , TPS7E71 , TPS7E72 , TPS7E81 , TPS7E82

 

  1.   1
  2. 1Introduction
  3. 2Adjustable Feedback Voltage
  4. 3Power Good
  5. 4Enable Logic
  6. 5Package Selection
  7. 6Controlled IQ In Dropout
  8. 7Transient Performance
  9. 8Summary

Transient Performance

Load transient performance describes the LDO’s ability to maintain the output voltage when the load changes. The key metrics are the voltage deviation (undershoot/overshoot) during a load-step and the settling time needed for the output to settle back within spec. Minimizing this peak in an LDO’s transient response can help shorten the time the regulator needs to bring its output back within the specified window, which in turn tightens the overall recovery time.
 Example Line Transient for LDOsFigure 6 Example Line Transient for LDOs
 Example Load Transient for LDOsFigure 7 Example Load Transient for LDOs
A line transient occurs when the input voltage changes abruptly, for example, when a battery's voltage sags under heavy use. A load transient occurs when the current demand from the circuit changes suddenly, like when a motor kicks on or a MCU wakes up from sleep mode. In both cases, the LDO's output voltage momentarily dips or spikes before regulating back to the target voltage. In battery-operated applications like power tools or home appliances, this matters because an unexpected voltage dip can trigger false fault conditions. An LDO with good transient response recovers from these disturbances quickly and with minimal voltage deviation, maintaining reliable operation even as the battery drains and loads switch on and off throughout normal use. See Table 3 for a comparison of transient performance across TI’s low IQ portfolio. Improving an LDO's transient response involves selecting the right type and value of output capacitor, as well as maintaining the error amplifier has sufficient bandwidth to react quickly to load steps.