See the following resources for further
information about the TI Code Generation Tools:
You can use the following books to
supplement this user's guide:
SPRU514
TMS320C28x Optimizing C/C++ Compiler User's Guide. Describes the TMS320C28x
C/C++ compiler. This C/C++ compiler accepts ANSI standard C/C++ source code and produces
assembly language source code for the TMS320C28x devices.
SPRU127
TMS320C2xx User's Guide. Discusses the hardware aspects of the TMS320C2xx
16-bit fixed-point digital signal processors. It describes the architecture, the
instruction set, and the on-chip peripherals.
SPRU430
TMS320C28x DSP CPU and Instruction Set Reference Guide. Describes the central
processing unit (CPU) and the assembly language instructions of the TMS320C28x
fixed-point CPU. It also describes emulation features available on these devices.
SPRU566
TMS320x28xx, 28xxx DSP Peripherals Reference Guide. Describes all the
peripherals available for TMS320x28xx and TMS320x28xxx devices.
https://www.ti.com/lit/pdf/SPRUHS1
TMS320C28x Extended Instruction Sets Technical Reference Manual
describes the architecture, pipeline, and instruction sets of the TMU, VCRC, VCU-II,
FPU32, and FPU64 accelerators.
SPRAC71
TMS320C28x Embedded Application Binary Interface Application Report. Provides a
specification for the ELF-based Embedded Application Binary Interface (EABI) for the
TMS320C28x family of processors from Texas Instruments. The EABI defines the low-level
interface between programs, program components, and the execution environment, including
the operating system if one is present.
SPRAAO8
Common Object File Format Application Report. Provides supplementary
information on the internal format of COFF object files. Much of this information
pertains to the symbolic debugging information that is produced by the C compiler.