SPRU513Y August 2001 – June 2022 SM320F28335-EP
In Section 9.10.1.2.2, the CRC algorithm is specified in the crc_table() operator. The specified algorithm is used to compute the CRC of the text data from b1.c.obj. The CRC tables generated by the linker are created in the special section .TI.crctab, which can be placed in the same manner as other sections. In this case, the CRC table _my_crc_table_for_b1 is created in section .TI.crctab:_my_crc_table_for_b1, and that section is placed in the CRCMEM memory region.