SPRUIU9C August 2020 – October 2025 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
The dual-bank Flash is partitioned as shown in Figure 4-1. Two sectors in each bank are allocated to the LFU bootloader, which comprises of Flash bank selection logic, the SCI kernel, and Flash APIs. These do not change during firmware upgrades. Bank 1 does not contain bank selection logic. The rest of the Flash sectors in the bank are allocated to the application. Bank selection logic allows the bootloader to determine which, if any, of the Flash banks are programmed with application firmware, and which bank contains the most recent application firmware version. Thus, bank selection logic is the entry point of the software system. The SCI kernel implements the transfer of the image from the host, and programming of Flash through Flash programming APIs (resident either in Flash or in ROM). A few locations in Sector 2 are reserved to store the below information: