SPRUIV4C May 2020 – December 2023
Floating-point division operations can be costly. Often, a division operation results in a run-time-support call to a predefined function that implements floating-point division. Such calls prevent software pipelining.
If your code divides by a constant
that is known at compile time,
consider pre-calculating the 1/constant
value and replacing the
division operation with a multiplication by 1/constant
. The
compiler automatically performs this optimization only if the
1/constant
value can be precisely represented in an IEEE-754
float or double.