SPRUIV4C May 2020 – December 2023
To maximize the efficiency of generated code, the C7000 compiler schedules as many instructions as possible in parallel, especially during software pipelining. To schedule instructions in parallel, the compiler must determine the relationships, or dependencies, between instructions. Dependency means that one instruction must occur before another; for example, a variable must be loaded from memory before it can be used. Because only independent instructions can execute in parallel, dependencies inhibit parallelism.