SPRUIV4C May 2020 – December 2023
Under certain limited circumstances, the compiler may generate two loops: one that assumes two pointers are not aliased and one that assumes the two pointers are aliased. It generates a run-time check to determine if the two pointers alias. This optimization is called run-time alias disambiguation. The advantage is that the loop that assumes no-aliased pointers can usually software pipeline at a much smaller initiation interval, leading to improved performance of the loop.
The compiler cannot always perform run-time alias disambiguation due to considerations that are too technical to describe here. In addition, certain further optimizations such as nested loop coalescing are inhibited when the compiler produces two different loops with a run-time alias check, so it is best to use the restrict keyword whenever legally possible.
For further discussion and details regarding identifying and eliminating loop-carried dependencies, consult the following references: