SPRUIY2A November 2024 – March 2025 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DU-Q1
INT sources are able to be masked, and the INT line can also be blocked/disabled by user code using the DSTS.INTE enable bit. If DSTS.INTE is enabled, then any interrupts received on the INT line are directly passed to the CPU for prioritization. Priority is then decided among the interrupts on the NMI or RTINT lines. To prevent an RTINT interrupt from nesting within a INT interrupt, the ATOMIC instruction can be used for a finite number of instruction packets.
On entering a INT ISR, further INTs are automatically disabled using the DSTS.INTE bit. To allow nesting, enable interrupts using the ENINT instruction. There also exists a DISINT instruction for disabling the INT line again.
The C29x CPU also provides a special INT called as Supervisor Interrupt. Supervisor Interrupt is essentially an INT which can override the DSTS.INTE setting. For example, Supervisor Interrupt can be a certain task monitor interrupt which requires the interrupt to not get blocked by erroneous setting of the DSTS.INTE.