SPRUIY9C May   2021  – December 2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Device Information
  6. 2Hardware
    1. 2.1 EVM Revisions and Assembly Variants
    2. 2.2 Important Usage Notes
    3. 2.3 System Description
      1. 2.3.1 Functional Block Diagram
      2. 2.3.2 Power-On/Off Procedures
        1. 2.3.2.1 Power-On Procedure
        2. 2.3.2.2 Power-Off Procedure
      3. 2.3.3 Peripheral and Major Component Description
        1. 2.3.3.1  Clocking
          1. 2.3.3.1.1 Ethernet PHY Clock
          2. 2.3.3.1.2 AM64x SoC Clock
        2. 2.3.3.2  Reset
        3. 2.3.3.3  Power
          1. 2.3.3.3.1 Power Input
          2. 2.3.3.3.2 USB Type-C Interface for Power Input
          3. 2.3.3.3.3 Power Fault Indication
          4. 2.3.3.3.4 Power Supply
          5. 2.3.3.3.5 Power Sequencing
          6. 2.3.3.3.6 Power Supply
        4. 2.3.3.4  Configuration
          1. 2.3.3.4.1 Boot Modes
        5. 2.3.3.5  JTAG
        6. 2.3.3.6  Test Automation
        7. 2.3.3.7  UART Interface
        8. 2.3.3.8  Memory Interfaces
          1. 2.3.3.8.1 LPDDR4 Interface
          2. 2.3.3.8.2 MMC Interface
            1. 2.3.3.8.2.1 Micro SD Interface
            2. 2.3.3.8.2.2 WiLink Interface
            3. 2.3.3.8.2.3 OSPI Interface
            4. 2.3.3.8.2.4 Board ID EEPROM Interface
        9. 2.3.3.9  Ethernet Interface
          1. 2.3.3.9.1 DP83867 PHY Default Configuration
          2. 2.3.3.9.2 DP83867 – Power, Clock, Reset, Interrupt and LEDs
          3. 2.3.3.9.3 Industrial Application LEDs
        10. 2.3.3.10 USB 3.0 Interface
        11. 2.3.3.11 PRU Connector
        12. 2.3.3.12 User Expansion Connector
        13. 2.3.3.13 MCU Connector
        14. 2.3.3.14 Interrupt
        15. 2.3.3.15 I2C Interface
        16. 2.3.3.16 IO Expander (GPIOs)
  7. 3Hardware Design Files
  8. 4Compliance Information
    1. 4.1 Regulatory Compliance
  9. 5Additional Information
    1. 5.1 Known Issues
      1. 5.1.1 Issue 1: LP8733x Max output Capacitance Spec Exceeded on LDO0 and LDO1
      2. 5.1.2 Issue 2: LP8733x Output Voltage of 0.9V Exceeds AM64x VDDR_CORE max Voltage Spec of 0.895 V
      3. 5.1.3 Issue 3 - SDIO Devices on MMC0 Require Careful Trace Lengths to Meet Interface Timing Requirements
      4. 5.1.4 Issue 4 - LPDDR4 Data Rate Limitation in Stressful Conditions
      5. 5.1.5 Issue 5 - Junk Character
      6. 5.1.6 Issue 6 - Test Power Down Signal Floating
      7. 5.1.7 Issue 7 - uSD Boot Not Working
    2.     Trademarks
    3.     65
  10. 6Revision History
Boot Modes

The boot mode for the SK EVM board is defined by two banks of switches, SW2 and SW3, or by the I2C buffer connected to the test automation connector. This allows for AM64x boot mode control by either the user (DIP Switch Control) or the test automation header. At the minimum, all the boot mode pins require a footprint for a pull-up or pull-down resistor. Any boot mode pin that must be toggled to support a needed boot mode must have a weak pull-down resistor and a switch (416131160808 from Wurth) capable of connecting a stronger pull-up resistor. The switch disconnects the pull-up resistor in the OFF position. For boot mode pins that are not controlled by switches, pull-up and pull-down resistor pads are included. Various boot modes for AM64x must be controlled by the user with the help of 8-Bit DIP switches. The following boot modes are supported by SK EVM:

  • OSPI
  • MMC1 - SD-Card
  • CSPW Ethernet
  • USB devices

The boot mode pins of the SoC have associated alternate functions during normal operation. Hence, isolation is provided using the Buffer IC to cater for alternate pin functionality. The output of the buffer is connected to the bootmode pins ON the AM64x and the output is enabled when the bootmode is needed during a reset cycle. The input to the buffer is connected to the DIP switch circuit and to the output of an I2C buffer set by the test automation circuit. If the test automation circuit is going to control the bootmode, then all the switches are manually set to the OFF position. The bootmode buffer are powered by an always ON power supply to make sure that the bootmode remains present even if the SoC power is cycled..

Figure 2-10 and Table 2-9 provide guidance to select the boot mode before the device is powered up.

SK-AM64 SK-AM64B Bootmode Switch Positions
                Example Figure 2-10 Bootmode Switch Positions Example
Table 2-9 BOOT-MODE Pin Mapping
Bit 15 Bit 14 Bit 13 Bit 12 Bit 11 Bit 10 Bit 9 Bit 8 Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0
Reserved Reserved Backup Boot Mode Configuration Backup Boot Mode Primary Boot Mode Configuration Primary Boot Mode PLL Configuration

• BOOT-MODE [0:2] – Denote system clock frequency for PLL configuration. By default, this bits are set for 25 MHz.

Table 2-10 gives details ON PLL reference clock selection.

Table 2-10 PLL Reference Clock Selection BOOTMODE [2:0]
SW3.6 SW3.7 SW3.8 PLL REF CLK (MHz)
OFF OFF OFF 19.2
OFF OFF ON 20
OFF ON OFF 24
OFF ON ON 25
ON OFF OFF 26
ON OFF ON 27
ON ON OFF Reserved
ON ON ON No PLL Configuration Done (slow speed backup)

• BOOT-MODE [3:6] – This provides primary boot mode configuration to select the requested boot mode after POR, that is, the peripheral/memory to boot from. Table 2-11 provides primary boot device selection details.

Table 2-11 Boot Device Selection BOOT-MODE [6:3]
SW3.2 SW3.3 SW3.4 SW3.5 Primary Boot Device Selected
OFF OFF OFF OFF Reserved
OFF OFF OFF ON OSPI
OFF OFF ON OFF QSPI
OFF OFF ON ON SPI
OFF ON OFF OFF Ethernet RGMII
OFF ON OFF ON Ethernet RMII
OFF ON ON OFF I2C
OFF ON ON ON UART
ON OFF OFF OFF MMC/SD card
ON OFF OFF ON emmc
ON OFF ON OFF USB
ON OFF ON ON Reserved
ON ON OFF OFF GPMC NOR
ON ON OFF ON PCIe
ON ON ON OFF xSPI
ON ON ON ON No boot/Dev Boot

• BOOT-MODE [10:12] – Select the backup boot mode, that is, the peripheral/memory to boot from, if primary boot device failed.

Table 2-12 provides backup boot mode selection details.

Table 2-12 Backup Boot Mode Selection BOOT-MODE [12:10]
SW2.4 SW2.5 SW2.6 Backup Boot Device Selected
OFF OFF OFF None (No backup mode)
OFF OFF ON USB
OFF ON OFF Reserved
OFF ON ON UART
ON OFF OFF Ethernet
ON OFF ON MMC/SD
ON ON OFF SPI
ON ON ON I2C

• BOOT-MODE [9:7] – These pins provide optional settings and are used in conjunction with the primary boot device selected.

Table 2-13 gives primary boot media configuration details.

Table 2-13 Primary Boot Media Configuration BOOT-MODE [9:7]
SW2.7 SW2.8 SW3.1 Boot Device
Reserved Reserved
Speed Iclk Csel OSPI
Reserved Iclk Csel QSPI
Reserved Mode Csel SPI
Clkout Delay Link stat Ethernet RGMII
Clkout Clk src Reserved Ethernet RMII
Bus Reset Reserved Addr I2C
Reserved Reserved UART
Port Reserved Fs/raw MMC/ SD card
Reserved voltage eMMC
Reserved Mode Lane swap USB
Reserved Reserved
Reserved GPMC NOR
Reserved Clocking PCIe
Speed Pin Cmd Csel xSPI
Reserved No/Dev No boot/Dev Boot

• BOOT-MODE [13] – These pins provide optional settings and are used in conjunction with the backup boot device devices. Switch SW2.6 when ON sets 1 and sets 0 if OFF, see the device-specific TRM.

• BOOT-MODE [14:15] – Reserved.

Table 2-14 provides backup boot media configuration options.

Table 2-14 Backup Boot Media Configuration BOOT-MODE [13]
SW2.3 Boot Device
Reserved None
Mode USB
Reserved Reserved
Reserved UART
IF Ethernet
Port MMC/SD
Reserved SPI
Reserved I2C