Select instances of the
module can
optionally route the low DAC output to an external pin to be used as an
external DAC. This is subject to the following constraints:
- This is available
only on select instances; consult the device data sheet to
determine if the CMPSS DAC has been pinned out for a
particular instance.
- In this case,
the DAC output is not available to the COMPL inside the
CMPSS module. The negative input to COMPL must be driven
from the device pin in this case, if used. All other CMPSS
module functionality, including the COMPH DAC source, is
usable in this case.
- See the device
data sheet for effective resolution of the CMPSS DAC
output.
Note: The
CMPSS low DAC output does not necessarily appear on the same pins
that are available for low comparator input. Consult the pinout of
the device data sheet to determine which pin the CMPSS output DAC is
available on.