SPRZ488D March 2022 – September 2023 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
CONTROLSS-CMPSS:Prescaler counter behaviour different from spec when DACSOURCE is made 0 or reconfigured as 1
While the prescaler is running if we make DACSOURCE = 0 the prescale counter will not reset and and if the enable condition is LOW the value stays and when the DACSOURCE is again configured as 1 the counter starts from the previous value which was retained. This bug is present only when DACSOURCE is configured during the prescale counter running.
Issue a soft reset between DACSOURCE configuration which is not a dynamic configuration.