SPRZ488F March 2022 – May 2026 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
CONTROLSS-ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set
If ADCINTSELxNx[INTxCONT] = 0, then interrupts will stop when the ADCINTFLG is set and no additional ADC interrupts will occur. When an ADC interrupt occurs simultaneously with a software write of the ADCINTFLGCLR register, the ADCINTFLG will unexpectedly remain set, blocking future ADC interrupts.
ADCINTSEL1N2[INT1CONT] = 1;
ADCINTSEL1N2[INT2CONT] = 1;
ADCINTSEL3N4[INT3CONT] = 1;
ADCINTSEL3N4[INT4CONT] = 1;AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT1) //ADCINT overflow
{
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 again
// If the ADCINTOVF condition will be ignored by the application
// then clear the flag here by writing 1 to ADCINTOVFCLR.
// If there is a ADCINTOVF handling routine, then either insert
// that code and clear the ADCINTOVF flag here or do not clear
// the ADCINTOVF here so the external routine will detect the
// condition.
// AdcaRegs.ADCINTOVFCLR.bit.ADCINT1 = 1; // clear OVF