SPRZ506E October 2022 – July 2025 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Revisions Affected: 0, A, B, C
Device security relies on the premise that unauthorized code is not allowed to enter the device and execute under any circumstances. To that end, the device provides two features that a user concerned about security should always enable.
When enabled in the USER OTP area of flash, the JTAGLOCK feature disables JTAG access (for example, debugger connection) to resources on the device, blocking an unauthorized party from using the JTAG interface to download any code into the device. When JTAGLOCK is enabled, the user can still allow an authorized party to unlock it by entering a password, or they can lock it permanently by programming a password value of all all-zeros.
The external bootloaders built into the TI ROM do not perform any authentication of the downloaded code. Enabling the Zero-pin boot option along with a flash boot mode in the USER OTP blocks all pin-based external bootloader options (for example, SCI, CAN, Parallel) from running at boot by forcing the boot process to jump immediately to internal flash after the base boot ROM execution concludes. For highest security, the Secure Flash boot mode can be chosen. This enables a precheck of the flash code by the base boot ROM before jumping to it.
If JTAG is locked permanently and the Zero-pin Boot to Flash option is enabled, programming tools that communicate with the device through JTAG or the built-in bootloaders will not work. If the ability to perform firmware upgrades is desired, the user must prestore code in flash to securely manage and perform the update.