STDA031 August 2026 TPS552892-Q1 , TPS61383-Q1
As an emergency power for collision unlocking, the supercapacitor needs to be charged to more than 90% of its rated voltage within a very short time after the vehicle is powered on, ensuring that the vehicle remains in a ready for emergency unlocking state throughout the journey. Different OEMs have different requirements for charging time, generally within 10s to 60s. Figure 3-1 shows the charging characteristic curve of the supercapacitor, divided into two stages: constant current (CC) charging and constant voltage (CV) charging. In CC stage, the main power supply charges the supercapacitor with a constant current, rapidly increasing the capacitor voltage. When the supercapacitor approaches a constant value, it automatically switches to constant voltage mode, limiting the charging current to prevent overvoltage damage to the capacitor while maintaining a fully charged state. The relationship between supercapacitor charging current and charging time is as below:
The larger the charging current, the shorter the charging time. Taking a 3s, 2.7V, 25F capacitor as an example, the equivalent capacitance is 8.3F. If it is necessary to charge the supercapacitor from 0V to the rated voltage of 8.1V within 10 seconds, the required charging current should be 6.7A. Considering the margin, it is necessary to select an IC that can support 7A constant current charging, such as TPS552892-Q1.
Figure 3-1 Supercapacitor Charging Characteristics