SWCS138G June 2017 – January 2025 TPS650864
PRODUCTION DATA
The buck controllers (BUCK1, BUCK2, and BUCK6) have inductor-valley current-limit architecture and the current limit is programmable by an external resistor at the ILIMx pin. Equation 1 shows the calculation for a desired resistor value, depending on specific application conditions. ILIMREF is the current source out of the ILIMx pin that is typically 50µA, and RDSON is the maximum channel resistance of the low-side FET. The scaling factor is 1.3 to take into account all errors and temperature variations of RDSON, ILIMREF, and RILIM. Finally, 8 is another scaling factor associated with ILIMREF.

where

where
The buck converter limit inductor peak current cycle-by-cycle to IIND_LIM is specified in Section 6.8.
The current limit circuit also protects against reverse current going back into the low side FET from the load. When operating in Force PWM mode, the inductor current is expected to go negative so it is important to ensure that the RILIM value is sufficient to account for this. If operating in PFM, this can be neglected. The equation for Force PWM minimum RILIM value is:

where
where
If RILIM is too low for the chosen inductor and voltage conditions, then the ripple current at no load triggers the negative current limit, forcing the low side FET to turn off. The irregular duty cycle created by the current limit triggering results in the output voltage increasing above target regulation point.