SWRA625B August   2018  – February 2020 CC1352P , CC1352R , CC2652P , CC2652R , CC2652R7 , CC2652RSIP

 

  1.   Z-Stack End Device Power Consumption Measurement With the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. 1 Introduction
    3. 2 Abbreviations and Acronyms
    4. 3 System Overview
      1. 3.1 Hardware:LAUNCHXL-CC1352P-2, LAUNCHXL-CC26X2R1
      2. 3.2 Software: Z-Stack
        1. 3.2.1 Z-Stack Development Environment
    5. 4 Measurement Setup
      1. 4.1 Instrumentation
      2. 4.2 Software Setup
        1. 4.2.1 Programming
        2. 4.2.2 ZC Node
        3. 4.2.3 ZED Node
        4. 4.2.4 GPD Node
        5. 4.2.5 Commissioning
    6. 5 Measurements
      1. 5.1 Measurements for Regular ZED
      2. 5.2 Measurements for Green Power Device
      3. 5.3 Measurements Using the EnergyTrace Tool
    7. 6 Application to a Practical Use Case
      1. 6.1 Estimation for Usage Scenario
        1. 6.1.1 Usage Scenario 1
      2. 6.2 Usage Scenario 2
    8. 7 Batteryless Green Power Device
    9. 8 Summary
    10. 9 References
  2.   Revision History

Z-Stack Development Environment

The measurement setup shown in Section 4 is based on the Z-Stack 3.3.1 Light Sink, Switch, and GPD Switch examples, which come as part of the SimpleLink CC13X2/CC26X2 Software Development Kit [5] described in [6].

In order to be able to compile the application and load onto the devices, the correct version of Code Composer Studio™ or IAR Embedded Workbench™ for ARM (mentioned in the Release Notes document inside the SimpleLink CC13X2/26X2 SDK install directory) must be installed, which can be obtained at http://www.ti.com/tool/CCSTUDIO or http://www.iar.com/downloads, respectively.