SWRA759 November 2022
Variable name: FREERTOS_INSTALL_DIR
Value: C:\ti\FreeRTOSv202107.00 (unzip folder address)
Figure 3-3 FreeRTOS Variable
Dialog in CCS
Figure 3-4 Installed Products
Dialog in CCSIf there is no available workspace when CCS is started, a dialog will pop up to ask to select a directory as workspace. Browse to the unzipped CC3235 Firmware folder and click ‘Launch’.
If a workspace in CCS is already opened, browse to the unzipped CC3235 Firmware folder in dialog from CCS->File->Switch Workspace->Other, and click ‘Launch’.
Figure 3-5 Launch Project in
CCS