SWRU633A September   2026  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Hardware and Debug Setup
      1. 2.2.1 Setup to use a LaunchPad as the Host Device
      2. 2.2.2 Setup to use the BoosterPack with SmartRF Studio 8
    3. 2.3 BoosterPack Connection Pinout
    4. 2.4 GPIO Connections for CC1407P
    5. 2.5 LEDs
    6. 2.6 RX SAW Filter
  9. 3Software
    1. 3.1 Getting Started
    2. 3.2 SmartRF Studio 8
      1. 3.2.1 Code Export from SmartRF Studio
    3. 3.3 Transceiver Firmware Update
    4. 3.4 Updating the Transceiver Firmware using SmartRF Studio 8
    5. 3.5 Updating the Transceiver Firmware using the ssbl_host Example
    6. 3.6 Porting Guidelines
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Known Hardware or Software Issues
    2.     Trademarks
  12. 6Revision History

Updating the Transceiver Firmware using SmartRF Studio 8

  1. Connect the CC1407P BoosterPack to the XDS110.
  2. Open SmartRF Studio 8.
  3. Under device selection, the CC140xP device and the current firmware version is shown (Figure 3-5).

    BP-CC1407P Device and Current Firmware Version

    Figure 3-5 Device and Current Firmware Version
  4. Select the "Update FW" button.
  5. SmartRF Studio for CC1407P includes a firmware version and is shown under "Included firmware version" (Figure 3-6). If the CC1407P needs to be updated with a different firmware, select "Firmware update binary file" and select the location of the binary file.

    BP-CC1407P Included Firmware Version

    Figure 3-6 Included Firmware Version
  6. Select "Update".
  7. If the update is successful, the message "Update completed successfully" is shown (Figure 3-7).

    BP-CC1407P Update Completed Successfully

    Figure 3-7 Update Completed Successfully
  8. In the main SmartRF Studio window, the new firmware version is shown for the device.

    BP-CC1407P New Firmware Version

    Figure 3-8 New Firmware Version