SWRU633A September   2026  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Hardware and Debug Setup
      1. 2.2.1 Setup to use a LaunchPad as the Host Device
      2. 2.2.2 Setup to use the BoosterPack with SmartRF Studio 8
    3. 2.3 BoosterPack Connection Pinout
    4. 2.4 GPIO Connections for CC1407P
    5. 2.5 LEDs
    6. 2.6 RX SAW Filter
  9. 3Software
    1. 3.1 Getting Started
    2. 3.2 SmartRF Studio 8
      1. 3.2.1 Code Export from SmartRF Studio
    3. 3.3 Transceiver Firmware Update
    4. 3.4 Updating the Transceiver Firmware using SmartRF Studio 8
    5. 3.5 Updating the Transceiver Firmware using the ssbl_host Example
    6. 3.6 Porting Guidelines
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Known Hardware or Software Issues
    2.     Trademarks
  12. 6Revision History

LEDs

The BoosterPack includes a red LED and a green LED. The LEDs can be controlled directly by the CC1407P or connected to GPIOs of the host device.

When two jumpers are placed on P2 as shown in Figure 2-6, the red LED is connected to DIO5, and the green LED is connected to DIO6. The CC1407P signals that can be routed to the LEDs are shown in Table 2-2.


BP-CC1407P LED Jumpers Mounted on P2

Figure 2-6 LED Jumpers Mounted on P2

When the two jumpers are removed as shown in Figure 2-7, a jumper cable can be placed on pin 1 of P2 to connect the red LED to a GPIO of the host device and on pin 3 to connect the green LED.

The examples in the SimpleLink Low Power Transceiver (TRX) plugin use the LEDs of the LaunchPad (host device) to indicate various events such as packet reception and packet transmission. These signals can instead be connected to the LEDs of the BoosterPack. Refer to the examples to know which DIOs of host device are being used for LED control.


BP-CC1407P LED Jumpers Removed from P2

Figure 2-7 LED Jumpers Removed from P2