SWRU633A September   2026  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Hardware and Debug Setup
      1. 2.2.1 Setup to use a LaunchPad as the Host Device
      2. 2.2.2 Setup to use the BoosterPack with SmartRF Studio 8
    3. 2.3 BoosterPack Connection Pinout
    4. 2.4 GPIO Connections for CC1407P
    5. 2.5 LEDs
    6. 2.6 RX SAW Filter
  9. 3Software
    1. 3.1 Getting Started
    2. 3.2 SmartRF Studio 8
      1. 3.2.1 Code Export from SmartRF Studio
    3. 3.3 Transceiver Firmware Update
    4. 3.4 Updating the Transceiver Firmware using SmartRF Studio 8
    5. 3.5 Updating the Transceiver Firmware using the ssbl_host Example
    6. 3.6 Porting Guidelines
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Known Hardware or Software Issues
    2.     Trademarks
  12. 6Revision History

Getting Started

The best way to start development with your CC1407P BoosterPack is to download the SimpleLink™ Low Power Transceiver (TRX) plugin. The plugin contains the host driver and examples implemented for the following F2 family devices:

  • CC1312R7
  • CC1352P7
  • CC2652R7
  • CC1314R10
  • CC1354P10

If you want to use the F2 example applications, you must first install the SimpleLink Low Power F2 SDK (install the version listed under "Dependencies" in the Plugins release note). After installing the SDK, install the plugin in the same directory as the SDK was installed by default (C:\ti).

The code examples for the CC1407P are found in the following location:

/simplelink_trx_plugin_x_xx_xx_xx\examples/rtos/LP_CCxxxx/trx_prop_rf/

Each example comes with a README.md file with detailed descriptions of the application. Please review the README file of the example you want to use.