SWRU633A September   2026  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Hardware and Debug Setup
      1. 2.2.1 Setup to use a LaunchPad as the Host Device
      2. 2.2.2 Setup to use the BoosterPack with SmartRF Studio 8
    3. 2.3 BoosterPack Connection Pinout
    4. 2.4 GPIO Connections for CC1407P
    5. 2.5 LEDs
    6. 2.6 RX SAW Filter
  9. 3Software
    1. 3.1 Getting Started
    2. 3.2 SmartRF Studio 8
      1. 3.2.1 Code Export from SmartRF Studio
    3. 3.3 Transceiver Firmware Update
    4. 3.4 Updating the Transceiver Firmware using SmartRF Studio 8
    5. 3.5 Updating the Transceiver Firmware using the ssbl_host Example
    6. 3.6 Porting Guidelines
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Known Hardware or Software Issues
    2.     Trademarks
  12. 6Revision History

Code Export from SmartRF Studio

The code export window can be used to export code structures to configure the device and is useful when you want to generate new PHY settings to integrate into an embedded project or change PHY settings for an existing code example.

The rfPacketTxGenFSK example from the TRX plugin runs default the 2gfsk50kbps PHY, but can easily be changed to run with a general purpose PHY generated using SmartRF Studio.

  1. Start by importing the rfPacketTxGenFSK from the TRX plugin to your example folder.

    Example: C:\CodeExamples\TRX\CC140xP

  2. Under PHY SELECTION in SmartRF Studio (see Figure 3-1).
    1. Select the General purpose GFSK.
    2. Select Create custom PHY, and implement any necessary changes (for this example we are changing the sync word).
    3. Press the "Code Export" button.

    BP-CC1407P Export Modified genFsk PHY

    Figure 3-1 Export Modified genFsk PHY
  3. Input the Output directory and Base file name for the new settings and select File->Save All (see Figure 3-2).

    BP-CC1407P File Name and Location for Code
              Export

    Figure 3-2 File Name and Location for Code Export
  4. Select the folder where you want to store the files (see Figure 3-3).

    BP-CC1407P Output Directory

    Figure 3-3 Output Directory
  5. Implement the below changes to the rfPacketTxGenFSK (see Figure 3-4).

    BP-CC1407P Necessary Code Changes

    Figure 3-4 Necessary Code Changes