SWRZ136B December   2023  – July 2025 CC2340R5-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Advisories Matrix
  5. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development Support-Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  6. 3Advisories
    1. 3.1  SPI_04
    2. 3.2  ADC_08
    3. 3.3  ADC_09
    4. 3.4  BATMON_01
    5. 3.5  BATMON_02
    6. 3.6  CKM_01
    7. 3.7  CLK_01
    8. 3.8  I2C_01
    9. 3.9  GPIO_01
    10. 3.10 PMU_01
    11. 3.11 UART_01
  7. 4Revision History

Device and Development Support-Tool Nomenclature

To designate the stages in the product development cycle, Texas Instruments™ stage identifiers for all devices and support tools. Devices are assigned one of two designators: X or P, to indicate non-production versions of the silicon die (for example, CC2340Q/R53/TI X). Fully qualified production versions carry no designator. Texas Instruments recommends two possible designators for its support tools: TMDX and TMDS. These designators represent evolutionary stages of product development from engineering prototypes (X/TMDX) through fully qualified production devices/tools (TMDS).

Device development evolutionary flow:

    XExperimental device that is not necessarily representative of the final device's electrical specifications and may not use production assembly flow
    PPrototype device that is not necessarily the final silicon die and may not necessarily meet final electrical specifications
    no designatorProduction version of the silicon die that is fully qualified

Support tool development evolutionary flow:

    TMDXDevelopment-support product that has not yet completed Texas Instruments internal qualification testing
    TMDSFully-qualified development-support product

X and P devices and TMDX development-support tools are shipped against the following disclaimer:

"Developmental product is intended for internal evaluation purposes."

Production devices and TMDS development-support tools have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.

Prototype devices (marked with X or P) have a greater failure rate than fully qualified production devices. Texas Instruments advises against their use in production systems, as their long-term reliability has not been fully characterized. Only fully qualified production devices should be used in end products.