TIDUET3 February 2021
The ISNS pin sets the overcurrent protection level. OCP1 is peak current protection level; OCP2 and OCP3 are average current protection levels. The threshold voltages are 0.425 V, 0.56 V, and 4.03 V, respectively. Set the OCP3 level at 140% of full load. Thus, the sensed average input current level at full load is given by:

The current sense ratio can then be calculated:

Select a current-sense capacitor first because there are fewer high-voltage capacitor choices than resistors. CISNS = 330 pF Then calculate the required ISNS resistor value: