TIDUF25 june 2023 ADS131M08 , MSPM0G1507
The MSPM0+ software used for evaluating this design is test software. This section discusses the features of the test software, which provides insight on how to implement custom software for metrology testing. This section discusses the setup of the ADS131M08 device and various peripherals on the MSPM0G3507 MCU. Subsequently, the metrology software is described as two major processes: the foreground process and background process.
The test data included in this reference design was taken using the generic test code written for the MSPM0G3507 MCU, which is a porting of the ADC Energy Metrology Library software to the TI MSPM0G-series of MCUs.
The original ADC Energy Metrology Library was developed and tested on an Arm Cortex-M4F MCU, which makes the software easily portable to popular Arm Cortex-M3, M4(F), and M33 microcontrollers, such as TI's wireless MCUs portfolio of Sub-1-GHz and 2.4-GHz devices.
The MSPM0+ software contains hardware abstraction layers which enable communication between the standalone ADC and an Arm Cortex-M0+ MCU and a library of metrology calculations for energy measurements. Also included in the software is a Microsoft Windows PC GUI to display metrology parameters from the TIDA-010243 reference design.