SLUSF65 October 2023 BQ25185
PRODUCTION DATA
When a valid input source is connected (VIN > VINDPM and VBAT +VSLEEP < VIN < VIN_OVP), the state of the CE pin and the TS/MR pin determines whether a charge cycle is initiated. When the CE pin is set to disable charging, VHOT < VTS/MR < VCOLD and a valid input source is connected, the battery FET is turned off, preventing any kind of charging of the battery. Note that supplement behavior is independent of the CE pin. The device will be able to charge a battery as long as VIN voltage is higher than the VINDPM threshold. This threshold is present as the VIN can be considered "powergood" with a very low battery voltage or a 0-V battery.
The following figure illustrates a typical charge cycle.