SNLS426F August 2012 – November 2018 DS125BR800
PRODUCTION DATA.
The DS125BR800 devices support reading directly from an external EEPROM device by implementing SMBus Master mode. When using the SMBus master mode, the DS125BR800 will read directly from specific location in the external EEPROM. When designing a system for using the external EEPROM, the user needs to follow these specific guidelines. For additional information, refer to SNLA228.
When tying multiple DS125BR800 devices to the SDA and SCL bus, use these guidelines to configure the devices.
Below is an example of a 2 kbits (256 x 8-bit) EEPROM in hex format for the DS125BR800 device. The first 3 bytes of the EEPROM always contain a header common and necessary to control initialization of all devices connected to the I2C bus. CRC enable flag to enable/disable CRC checking. If CRC checking is disabled, a fixed pattern (8’hA5) is written/read instead of the CRC byte from the CRC location, to simplify the control. There is a MAP bit to flag the presence of an address map that specifies the configuration data start in the EEPROM. If the MAP bit is not present the configuration data start address is derived from the DS125BR800 address and the configuration data size. A bit to indicate an EEPROM size > 256 bytes is necessary to properly address the EEPROM. There are 37 bytes of data size for each DS125BR800 device. For additional information on EEPROM programming, refer to SNLA228.
spacer
:2000000000001000000407002FAD4002FAD4002FAD4002FAD401805F5A8005F5A8005F5AD8
:200020008005F5A800005454000000000000000000000000000000000000000000000000F6
:20006000000000000000000000000000000000000000000000000000000000000000000080
:20008000000000000000000000000000000000000000000000000000000000000000000060
:2000A000000000000000000000000000000000000000000000000000000000000000000040
:2000C000000000000000000000000000000000000000000000000000000000000000000020
:2000E000000000000000000000000000000000000000000000000000000000000000000000
:200040000000000000000000000000000000000000000000000000000000000000000000A0
NOTE
The maximum EEPROM size supported is 8-kbits (1024 x 8 bits).
EEPROM Address Byte | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | BIt 0 | ||
---|---|---|---|---|---|---|---|---|---|---|
Description | 0x00 | CRC EN | Address Map Present | EEPROM > 256 Bytes | Reserved | DEVICE COUNT[3] | DEVICE COUNT[2] | DEVICE COUNT[1] | DEVICE COUNT[0] | |
Default Value | 0x00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x01 | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | |
Default Value | 0x00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x02 | Max EEPROM Burst size[7] | Max EEPROM Burst size[6] | Max EEPROM Burst size[5] | Max EEPROM Burst size[4] | Max EEPROM Burst size[3] | Max EEPROM Burst size[2] | Max EEPROM Burst size[1] | Max EEPROM Burst size[0] | |
Default Value | 0x00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x03 | PWDN_ch7 | PWDN_ch6 | PWDN_ch5 | PWDN_ch4 | PWDN_ch3 | PWDN_ch2 | PWDN_ch1 | PWDN_ch0 | |
SMBus Register | 0x01 [7] | 0x01 [6] | 0x01 [5] | 0x01 [4] | 0x01 [3] | 0x01 [2] | 0x01 [1] | 0x01 [0] | ||
Default Value | 0x00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x04 | lpbk_1 | lpbk_0 | PWDN_INPUTS | PWDN_OSC | Ovrd_PWDN | Reserved | Reserved | Reserved | |
SMBus Register | 0x02 [5] | 0x02 [4] | 0x02 [3] | 0x02 [2] | 0x02 [0] | 0x04 [7] | 0x04 [6] | 0x04 [5] | ||
Default Value | 00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x05 | Reserved | Reserved | Reserved | Reserved | Reserved | rxdet_btb_en | Ovrd_idle_th | Ovrd_RES | |
SMBus Register | 0x04 [4] | 0x04 [3] | 0x04 [2] | 0x04 [1] | 0x04 [0] | 0x06 [4] | 0x08 [6] | 0x08 [5] | ||
Default Value | 04 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | |
Description | 0x06 | Ovrd_IDLE | Ovrd_RX_DET | Ovrd_MODE | Ovrd_RES | Ovrd_RES | rx_delay_sel_2 | rx_delay_sel_1 | rx_delay_sel_0 | |
SMBus Register | 0x08 [4] | 0x08 [3] | 0x08 [2] | 0x08 [1] | 0x08 [0] | 0x0B [6] | 0x0B [5] | 0x0B [4] | ||
Default Value | 07 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | |
Description | 0x07 | RD_delay_sel_3 | RD_delay_sel_2 | RD_delay_sel_1 | RD_delay_sel_0 | ch0_Idle_auto | ch0_Idle_sel | ch0_RXDET_1 | ch0_RXDET_0 | |
SMBus Register | 0x0B [3] | 0x0B [2] | 0x0B [1] | 0x0B [0] | 0x0E [5] | 0x0E [4] | 0x0E [3] | 0x0E [2] | ||
Default Value | 00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x08 | ch0_BST_7 | ch0_BST_6 | ch0_BST_5 | ch0_BST_4 | ch0_BST_3 | ch0_BST_2 | ch0_BST_1 | ch0_BST_0 | |
SMBus Register | 0x0F [7] | 0x0F [6] | 0x0F [5] | 0x0F [4] | 0x0F [3] | 0x0F [2] | 0x0F [1] | 0x0F [0] | ||
Default Value | 2F | 0 | 0 | 1 | 0 | 1 | 1 | 1 | 1 | |
Description | 0x09 | ch0_Sel_scp | ch0_Sel_mode | ch0_RES_2 | ch0_RES_1 | ch0_RES_0 | ch0_VOD_2 | ch0_VOD_1 | ch0_VOD_0 | |
SMBus Register | 0x10 [7] | 0x10 [6] | 0x10 [5] | 0x10 [4] | 0x10 [3] | 0x10 [2] | 0x10 [1] | 0x10 [0] | ||
Default Value | AD | 1 | 0 | 1 | 0 | 1 | 1 | 0 | 1 | |
Description | 0x0A | ch0_DEM_2 | ch0_DEM_1 | ch0_DEM_0 | ch0_Slow | ch0_idle_tha_1 | ch0_idle_tha_0 | ch0_idle_thd_1 | ch0_idle_thd_0 | |
SMBus Register | 0x11 [2] | 0x11 [1] | 0x11 [0] | 0x12 [7] | 0x12 [3] | 0x12 [2] | 0x12 [1] | 0x12 [0] | ||
Default Value | 40 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x0B | ch1_Idle_auto | ch1_Idle_sel | ch1_RXDET_1 | ch1_RXDET_0 | ch1_BST_7 | ch1_BST_6 | ch1_BST_5 | ch1_BST_4 | |
SMBus Register | 0x15 [5] | 0x15 [4] | 0x15 [3] | 0x15 [2] | 0x16 [7] | 0x16 [6] | 0x16 [5] | 0x16 [4] | ||
Default Value | 02 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | |
Description | 0x0C | ch1_BST_3 | ch1_BST_2 | ch1_BST_1 | ch1_BST_0 | ch1_Sel_scp | ch1_Sel_mode | ch1_RES_2 | ch1_RES_1 | |
SMBus Register | 0x16 [3] | 0x16 [2] | 0x16 [1] | 0x16 [0] | 0x17 [7] | 0x17 [6] | 0x17 [5] | 0x17 [4] | ||
Default Value | FA | 1 | 1 | 1 | 1 | 1 | 0 | 1 | 0 | |
Description | 0x0D | ch1_RES_0 | ch1_VOD_2 | ch1_VOD_1 | ch1_VOD_0 | ch1_DEM_2 | ch1_DEM_1 | ch1_DEM_0 | ch1_Slow | |
SMBus Register | 0x17 [3] | 0x17 [2] | 0x17 [1] | 0x17 [0] | 0x18 [2] | 0x18 [1] | 0x18 [0] | 0x19 [7] | ||
Default Value | 2F | 1 | 1 | 0 | 1 | 0 | 1 | 0 | 0 | |
Description | 0x0E | ch1_idle_tha_1 | ch1_idle_tha_0 | ch1_idle_thd_1 | ch1_idle_thd_0 | ch2_Idle_auto | ch2_Idle_sel | ch2_RXDET_1 | ch2_RXDET_0 | |
SMBus Register | 0x19 [3] | 0x19 [2] | 0x19 [1] | 0x19 [0] | 0x1C [5] | 0x1C [4] | 0x1C [3] | 0x1C [2] | ||
Default Value | 00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x0F | ch2_BST_7 | ch2_BST_6 | ch2_BST_5 | ch2_BST_4 | ch2_BST_3 | ch2_BST_2 | ch2_BST_1 | ch2_BST_0 | |
SMBus Register | 0x1D [7] | 0x1D [6] | 0x1D [5] | 0x1D [4] | 0x1D [3] | 0x1D [2] | 0x1D [1] | 0x1D [0] | ||
Default Value | 2F | 0 | 0 | 1 | 0 | 1 | 1 | 1 | 1 | |
Description | 0x10 | ch2_Sel_scp | ch2_Sel_mode | ch2_RES_2 | ch2_RES_1 | ch2_RES_0 | ch2_VOD_2 | ch2_VOD_1 | ch2_VOD_0 | |
SMBus Register | 0x1E [7] | 0x1E [6] | 0x1E [5] | 0x1E [4] | 0x1E [3] | 0x1E [2] | 0x1E [1] | 0x1E [0] | ||
Default Value | AD | 1 | 0 | 1 | 0 | 1 | 1 | 0 | 1 | |
Description | 0x11 | ch2_DEM_2 | ch2_DEM_1 | ch2_DEM_0 | ch2_Slow | ch2_idle_tha_1 | ch2_idle_tha_0 | ch2_idle_thd_1 | ch2_idle_thd_0 | |
SMBus Register | 0x1F [2] | 0x1F [1] | 0x1F [0] | 0x20 [7] | 0x20 [3] | 0x20 [2] | 0x20 [1] | 0x20 [0] | ||
Default Value | 40 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x12 | ch3_Idle_auto | ch3_Idle_sel | ch3_RXDET_1 | ch3_RXDET_0 | ch3_BST_7 | ch3_BST_6 | ch3_BST_5 | ch3_BST_4 | |
SMBus Register | 0x23 [5] | 0x23 [4] | 0x23 [3] | 0x23 [2] | 0x24 [7] | 0x24 [6] | 0x24 [5] | 0x24 [4] | ||
Default Value | 02 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | |
Description | 0x13 | ch3_BST_3 | ch3_BST_2 | ch3_BST_1 | ch3_BST_0 | ch3_Sel_scp | ch3_Sel_mode | ch3_RES_2 | ch3_RES_1 | |
SMBus Register | 0x24 [3] | 0x24 [2] | 0x24 [1] | 0x24 [0] | 0x25 [7] | 0x25 [6] | 0x25 [5] | 0x25 [4] | ||
Default Value | FA | 1 | 1 | 1 | 1 | 1 | 0 | 1 | 0 | |
Description | 0x14 | ch3_RES_0 | ch3_VOD_2 | ch3_VOD_1 | ch3_VOD_0 | ch3_DEM_2 | ch3_DEM_1 | ch3_DEM_0 | ch3_Slow | |
SMBus Register | 0x25 [3] | 0x25 [2] | 0x25 [1] | 0x25 [0] | 0x26 [2] | 0x26 [1] | 0x26 [0] | 0x27 [7] | ||
Default Value | D4 | 1 | 1 | 0 | 1 | 0 | 1 | 0 | 0 | |
Description | 0x15 | ch3_idle_tha_1 | ch3_idle_tha_0 | ch3_idle_thd_1 | ch3_idle_thd_0 | ovrd_fast_idle | en_high_idle_th_n | en_high_idle_th_s | en_fast_idle_n | |
SMBus Register | 0x27 [3] | 0x27 [2] | 0x27 [1] | 0x27 [0] | 0x28 [6] | 0x28 [5] | 0x28 [4] | 0x28 [3] | ||
Default Value | 09 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | |
Description | 0x16 | en_fast_idle_s | eqsd_mgain_n | eqsd_mgain_s | ch4_Idle_auto | ch4_Idle_sel | ch4_RXDET_1 | ch4_RXDET_0 | ch4_BST_7 | |
SMBus Register | 0x28 [2] | 0x28 [1] | 0x28 [0] | 0x2B [5] | 0x2B [4] | 0x2B [3] | 0x2B [2] | 0x2C [7] | ||
Default Value | 80 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x17 | ch4_BST_6 | ch4_BST_5 | ch4_BST_4 | ch4_BST_3 | ch4_BST_2 | ch4_BST_1 | ch4_BST_0 | ch4_Sel_scp | |
SMBus Register | 0x2C [6] | 0x2C [5] | 0x2C [4] | 0x2C [3] | 0x2C [2] | 0x2C [1] | 0x2C [0] | 0x2D [7] | ||
Default Value | 5F | 0 | 1 | 0 | 1 | 1 | 1 | 1 | 1 | |
Description | 0x18 | ch4_Sel_mode | ch4_RES_2 | ch4_RES_1 | ch4_RES_0 | ch4_VOD_2 | ch4_VOD_1 | ch4_VOD_0 | ch4_DEM_2 | |
SMBus Register | 0x2D [6] | 0x2D [5] | 0x2D [4] | 0x2D [3] | 0x2D [2] | 0x2D [1] | 0x2D [0] | 0x2E [2] | ||
Default Value | 5A | 0 | 1 | 0 | 1 | 1 | 0 | 1 | 0 | |
Description | 0x19 | ch4_DEM_1 | ch4_DEM_0 | ch4_Slow | ch4_idle_tha_1 | ch4_idle_tha_0 | ch4_idle_thd_1 | ch4_idle_thd_0 | ch5_Idle_auto | |
SMBus Register | 0x2E [1] | 0x2E [0] | 0x2F [7] | 0x2F [3] | 0x2F [2] | 0x2F [1] | 0x2F [0] | 0x32 [5] | ||
Default Value | 80 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x1A | ch5_Idle_sel | ch5_RXDET_1 | ch5_RXDET_0 | ch5_BST_7 | ch5_BST_6 | ch5_BST_5 | ch5_BST_4 | ch5_BST_3 | |
SMBus Register | 0x32 [4] | 0x32 [3] | 0x32 [2] | 0x33 [7] | 0x33 [6] | 0x33 [5] | 0x33 [4] | 0x33 [3] | ||
Default Value | 05 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 1 | |
Description | 0x1B | ch5_BST_2 | ch5_BST_1 | ch5_BST_0 | ch5_Sel_scp | ch5_Sel_mode | ch5_RES_2 | ch5_RES_1 | ch5_RES_0 | |
SMBus Register | 0x33 [2] | 0x33 [1] | 0x33 [0] | 0x34 [7] | 0x34 [6] | 0x34 [5] | 0x34 [4] | 0x34 [3] | ||
Default Value | F5 | 1 | 1 | 1 | 1 | 0 | 1 | 0 | 1 | |
Description | 0x1C | ch5_VOD_2 | ch5_VOD_1 | ch5_VOD_0 | ch5_DEM_2 | ch5_DEM_1 | ch5_DEM_0 | ch5_Slow | ch5_idle_tha_1 | |
SMBus Register | 0x34 [2] | 0x34 [1] | 0x34 [0] | 0x35 [2] | 0x35 [1] | 0x35 [0] | 0x36 [7] | 0x36 [3] | ||
Default Value | A8 | 1 | 0 | 1 | 0 | 1 | 0 | 0 | 0 | |
Description | 0x1D | ch5_idle_tha_0 | ch5_idle_thd_1 | ch5_idle_thd_0 | ch6_Idle_auto | ch6_Idle_sel | ch6_RXDET_1 | ch6_RXDET_0 | ch6_BST_7 | |
SMBus Register | 0x36 [2] | 0x36 [1] | 0x36 [0] | 0x39 [5] | 0x39 [4] | 0x39 [3] | 0x39 [2] | 0x3A [7] | ||
Default Value | 00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x1E | ch6_BST_6 | ch6_BST_5 | ch6_BST_4 | ch6_BST_3 | ch6_BST_2 | ch6_BST_1 | ch6_BST_0 | ch6_Sel_scp | |
SMBus Register | 0x3A [6] | 0x3A [5] | 0x3A [4] | 0x3A [3] | 0x3A [2] | 0x3A [1] | 0x3A [0] | 0x3B [7] | ||
Default Value | 5F | 0 | 1 | 0 | 1 | 1 | 1 | 1 | 1 | |
Description | 0x1F | ch6_Sel_mode | ch6_RES_2 | ch6_RES_1 | ch6_RES_0 | ch6_VOD_2 | ch6_VOD_1 | ch6_VOD_0 | ch6_DEM_2 | |
SMBus Register | 0x3B [6] | 0x3B [5] | 0x3B [4] | 0x3B [3] | 0x3B [2] | 0x3B [1] | 0x3B [0] | 0x3C [2] | ||
Default Value | 5A | 0 | 1 | 0 | 1 | 1 | 0 | 1 | 0 | |
Description | 0x20 | ch6_DEM_1 | ch6_DEM_0 | ch6_Slow | ch6_idle_tha_1 | ch6_idle_tha_0 | ch6_idle_thd_1 | ch6_idle_thd_0 | ch7_Idle_auto | |
SMBus Register | 0x3C [1] | 0x3C [0] | 0x3D [7] | 0x3D [3] | 0x3D [2] | 0x3D [1] | 0x3D [0] | 0x40 [5] | ||
Default Value | 80 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x21 | ch7_Idle_sel | ch7_RXDET_1 | ch7_RXDET_0 | ch7_BST_7 | ch7_BST_6 | ch7_BST_5 | ch7_BST_4 | ch7_BST_3 | |
SMBus Register | 0x40 [4] | 0x40 [3] | 0x40 [2] | 0x41 [7] | 0x41 [6] | 0x41 [5] | 0x41 [4] | 0x41 [3] | ||
Default Value | 05 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 1 | |
Description | 0x22 | ch7_BST_2 | ch7_BST_1 | ch7_BST_0 | ch7_Sel_scp | ch7_Sel_mode | ch7_RES_2 | ch7_RES_1 | ch7_RES_0 | |
SMBus Register | 0x41 [2] | 0x41 [1] | 0x41 [0] | 0x42 [7] | 0x42 [6] | 0x42 [5] | 0x42 [4] | 0x42 [3] | ||
Default Value | F5 | 1 | 1 | 1 | 1 | 0 | 1 | 0 | 1 | |
Description | 0x23 | ch7_VOD_2 | ch7_VOD_1 | ch7_VOD_0 | ch7_DEM_2 | ch7_DEM_1 | ch7_DEM_0 | ch7_Slow | ch7_idle_tha_1 | |
SMBus Register | 0x42 [2] | 0x42 [1] | 0x42 [0] | 0x43 [2] | 0x43 [1] | 0x43 [0] | 0x44 [7] | 0x44 [3] | ||
Default Value | A8 | 1 | 0 | 1 | 0 | 1 | 0 | 0 | 0 | |
Description | 0x24 | ch7_idle_tha_0 | ch7_idle_thd_1 | ch7_idle_thd_0 | Reserved | Reserved | Reserved | Reserved | Reserved | |
SMBus Register | 0x44 [2] | 0x44 [1] | 0x44 [0] | 0x47 [3] | 0x47 [2] | 0x47 [2] | 0x47 [0] | 0x48 [7] | ||
Default Value | 00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x25 | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | |
SMBus Register | 0x48 [6] | 0x4C [7] | 0x4C [6] | 0x4C [5] | 0x4C [4] | 0x4C [3] | 0x4C [0] | 0x59 [0] | ||
Default Value | 00 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Description | 0x26 | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | |
SMBus Register | 0x5A [7] | 0x5A [6] | 0x5A [5] | 0x5A [4] | 0x5A [3] | 0x5A [2] | 0x5A [1] | 0x5A [0] | ||
Default Value | 54 | 0 | 1 | 0 | 1 | 0 | 1 | 0 | 0 | |
Description | 0x27 | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | |
SMBus Register | 0x5B [7] | 0x5B [6] | 0x5B [5] | 0x5B [4] | 0x5B [3] | 0x5B [2] | 0x5B [1] | 0x5B [0] | ||
Default Value | 54 | 0 | 1 | 0 | 1 | 0 | 1 | 0 | 0 |
EEPROM Address | Address (Hex) | EEPROM Data | Comments |
---|---|---|---|
0 | 00 | 0x43 | CRC_EN = 0, Address Map = 1, >256 bytes = 0, Device Count[3:0] = 3 |
1 | 01 | 0x00 | |
2 | 02 | 0x08 | EEPROM Burst Size |
3 | 03 | 0x00 | CRC not used |
4 | 04 | 0x0B | Device 0 Address Location |
5 | 05 | 0x00 | CRC not used |
6 | 06 | 0x0B | Device 1 Address Location |
7 | 07 | 0x00 | CRC not used |
8 | 08 | 0x30 | Device 2 Address Location |
9 | 09 | 0x00 | CRC not used |
10 | 0A | 0x30 | Device 3 Address Location |
11 | 0B | 0x00 | Begin Device 0, 1 - Address Offset 3 |
12 | 0C | 0x00 | |
13 | 0D | 0x04 | |
14 | 0E | 0x07 | |
15 | 0F | 0x00 | |
16 | 10 | 0x00 | EQ CHB0 = 00 |
17 | 11 | 0xAB | VOD CHB0 = 1.0 V |
18 | 12 | 0x00 | DEM CHB0 = 0 (0 dB) |
19 | 13 | 0x00 | EQ CHB1 = 00 |
20 | 14 | 0x0A | VOD CHB1 = 1.0 V |
21 | 15 | 0xB0 | DEM CHB1 = 0 (0 dB) |
22 | 16 | 0x00 | |
23 | 17 | 0x00 | EQ CHB2 = 00 |
24 | 18 | 0xAB | VOD CHB2 = 1.0 V |
25 | 19 | 0x00 | DEM CHB2 = 0 (0 dB) |
26 | 1A | 0x00 | EQ CHB3 = 00 |
27 | 1B | 0x0A | VOD CHB3 = 1.0 V |
28 | 1C | 0xB0 | DEM CHB3 = 0 (0 dB) |
29 | 1D | 0x01 | |
30 | 1E | 0x80 | |
31 | 1F | 0x01 | EQ CHA0 = 00 |
32 | 20 | 0x56 | VOD CHA0 = 1.0 V |
33 | 21 | 0x00 | DEM CHA0 = 0 (0 dB) |
34 | 22 | 0x00 | EQ CHA1 = 00 |
35 | 23 | 0x15 | VOD CHA1 = 1.0 V |
36 | 24 | 0x60 | DEM CHA1 = 0 (0 dB) |
37 | 25 | 0x00 | |
38 | 26 | 0x01 | EQ CHA2 = 00 |
39 | 27 | 0x56 | VOD CHA2 = 1.0 V |
40 | 28 | 0x00 | DEM CHA2 = 0 (0 dB) |
41 | 29 | 0x00 | EQ CHA3 = 00 |
42 | 2A | 0x15 | VOD CHA3 = 1.0 V |
43 | 2B | 0x60 | DEM CHA3 = 0 (0 dB) |
44 | 2C | 0x00 | |
45 | 2D | 0x00 | |
46 | 2E | 0x54 | |
47 | 2F | 0x54 | End Device 0, 1 - Address Offset 39 |
48 | 30 | 0x00 | Begin Device 2, 3 - Address Offset 3 |
49 | 31 | 0x00 | |
50 | 32 | 0x04 | |
51 | 33 | 0x07 | |
52 | 34 | 0x00 | |
53 | 35 | 0x00 | EQ CHB0 = 00 |
54 | 36 | 0xAB | VOD CHB0 = 1.0 V |
55 | 37 | 0x00 | DEM CHB0 = 0 (0 dB) |
56 | 38 | 0x00 | EQ CHB1 = 00 |
57 | 39 | 0x0A | VOD CHB1 = 1.0 V |
58 | 3A | 0xB0 | DEM CHB1 = 0 (0 dB) |
59 | 3B | 0x00 | |
60 | 3C | 0x00 | EQ CHB2 = 00 |
61 | 3D | 0xAB | VOD CHB2 = 1.0 V |
62 | 3E | 0x00 | DEM CHB2 = 0 (0 dB) |
63 | 3F | 0x00 | EQ CHB3 = 00 |
64 | 40 | 0x0A | VOD CHB3 = 1.0 V |
65 | 41 | 0xB0 | DEM CHB3 = 0 (0 dB) |
66 | 42 | 0x01 | |
67 | 43 | 0x80 | |
68 | 44 | 0x01 | EQ CHA0 = 00 |
69 | 45 | 0x56 | VOD CHA0 = 1.0 V |
70 | 46 | 0x00 | DEM CHA0 = 0 (0 dB) |
71 | 47 | 0x00 | EQ CHA1 = 00 |
72 | 48 | 0x15 | VOD CHA1 = 1.0 V |
73 | 49 | 0x60 | DEM CHA1 = 0 (0 dB) |
74 | 4A | 0x00 | |
75 | 4B | 0x01 | EQ CHA2 = 00 |
76 | 4C | 0x56 | VOD CHA2 = 1.0 V |
77 | 4D | 0x00 | DEM CHA2 = 0 (0 dB) |
78 | 4E | 0x00 | EQ CHA3 = 00 |
79 | 4F | 0x15 | VOD CHA3 = 1.0 V |
80 | 50 | 0x60 | DEM CHA3 = 0 (0 dB) |
81 | 51 | 0x00 | |
82 | 52 | 0x00 | |
83 | 53 | 0x54 | |
84 | 54 | 0x54 | End Device 2, 3 - Address Offset 39 |
NOTE: CRC_EN = 0, Address Map = 1, >256 byte = 0, Device Count[3:0] = 3. This example has all 8 channels set to EQ = 00 (min boost), VOD = 1.0 V, DEM = 0 (0 dB) and multiple device can point to the same address map. Maximum EEPROM size is 8kbits (1024 x 8-bits).