SCDS459A October 2022 – November 2022 TMUX7436F
PRODMIX
Source on-leakage current (IS(ON)) and drain on-leakage current (ID(ON)) denote the channel leakage currents when the switch is in the on state. IS(ON) is measured with the drain floating, while ID(ON) is measured with the source floating. Figure 7-3 shows the circuit used for measuring the on-leakage currents.