JAJSHX5F October 2010 – September 2019 ADS1118
PRODUCTION DATA.
The data in a 32-bit data transmission cycle consists of four bytes: two bytes for the conversion result, and an additional two bytes for the Config Register read back. The device always reads the MSB first.
Write the same Config register setting twice during one transmission cycle as shown in Figure 40. If convenient, write the Config register setting once during the first half of the transmission cycle, and then hold the DIN pin either low (as shown in Figure 41) or high during the second half of the cycle. If no update to the Config register is required, hold the DIN pin either low or high during the entire transmission cycle. The Config register setting written in the first two bytes of a 32-bit transmission cycle is read back in the last two bytes of the same cycle.