JAJSRR3 October 2023 BQ25185
PRODUCTION DATA
The device will perform factory mode entry when the pushbutton is pressed (TS/MR is held low) for a time tLPRESS while a valid input is present, then removing VIN once the duration is met. Factory Mode is a low IQ state that turns off the SYS regulation to minimize battery consumption Toggling the /CE pin will restart the timer for the long press button when VIN is present.
To wake up the device from factory mode, insert a valid VIN. The TS/MR push button cannot be used to wake from Factory Mode.