JAJSLA9E may 2015 – april 2023 DLP7000UV
PRODUCTION DATA
The DLP7000UV has only one functional mode, it is set to be highly optimized for low latency and high speed in generating mirror clocking pulses and timings.
When operated with the DLPC410 controller in conjunction with the DLPA200 driver, the DLP7000UV can be operated in several display modes. The DLP7000UV is loaded as 16 blocks of 48 rows each. Figure 8-7, Figure 8-8, Figure 8-9, and Figure 8-10 show how the image is loaded by the different Micromirror Clocking Pulse modes.
There are four Micromirror Clocking Pulse modes that determine which blocks are reset when a Micromirror Clocking Pulse command is issued: