JAJSIP7D September 2015 – September 2020 DLPC910
PRODUCTION DATA
The controller reset input CTRL_RSTZ is an active low, asynchronous reset. This reset can be sourced from a voltage supervisor or from the customer interface. Users should note that the chipset will not operate correctly if all DLPC910 power supplies are not in range at the time this reset is released.