JAJSA67I April 2004 – February 2019 LM2743
PRODUCTION DATA.
In the case where extra protection is used to help an output short condition, a current foldback resistor (RCLF) should be considered, see Figure 29. First select the percentage of current limit foldback (PLIM):
where P is a ratio between 0 and 1.
Obtain the RCS with the following equation:
where ISEN = 40 μA. If the switch node goes above 9.5 V the following criterion must be satisfied:
The equation for calculating the foldback resistance value is: