JAJSR90 September 2023 LMQ644A2-Q1
PRODMIX
The frequency is set using a resistor on the RT pin. A resistor to AGND is used to set the adjustable operating frequency. See below for resistor values. Note that if a resistor value falls outside of the recommended range, it can cause the device to stop switching. Do not apply a pulsed signal to this pin to force synchronization. If synchronization is needed, see the SYNC pin.
For example, for fSW = 400 kHz, RT = (16.4 / 0.4) - 0.633 = 40.37, so a 40.2-kΩ resistor is selected as the closest choice.
RT (kΩ) |
Frequency (kHz) |
---|---|
6.81 | 2206 |
7.15 |
2106 |
15.4 |
1005 |
31.6 |
497.4 |
39.2 |
402 |
158 |
101 |