JAJSPJ0C August 2005 – December 2022 SN74LVCH8T245
PRODUCTION DATA
Calculate the enable times for the SN74LVCH8T245 using Equation 1, Equation 2, Equation 3, and Equation 4:
In a bidirectional application, these enable times provide the maximum delay from the time the DIR bit is switched until an output is expected. For example, if the device initially is transmitting from A to B, then the DIR bit is switched; the B port of the device must be disabled before presenting it with an input. After the B port has been disabled, an input signal applied to it appears on the corresponding A port after the specified propagation delay.