JAJSK40F May 2009 – January 2023 TCA6416A
PRODUCTION DATA
The bus controller first must send the TCA6416A address with the LSB set to a logic 0 (see GUID-00086FD5-7B10-4430-85E2-7F1994D974B9.html#SCPS133IMG2619 for device address). The command byte is sent after the address and determines which register is accessed.
After a restart, the device address is sent again but, this time, the LSB is set to a logic 1. Data from the register defined by the command byte then is sent by the TCA6416A (see #SCPS133IMG6461 and #SCPS133IMG9375).
After a restart, the value of the register defined by the command byte matches the register being accessed when the restart occurred. For example, if the command byte references Input Port 1 before the restart, and the restart occurs when Input Port 0 is being read, the stored command byte changes to reference Input Port 0. The original command byte is forgotten. If a subsequent restart occurs, Input Port 0 is read first. Data is clocked into the register on the rising edge of the ACK clock pulse. After the first byte is read, additional bytes may be read, but the data now reflects the information in the other register in the pair. For example, if Input Port 1 is read, the next byte read is Input Port 0.
Data is clocked into the register on the rising edge of the ACK clock pulse. There is no limitation on the number of data bytes received in one read transmission, but when the final byte is received, the bus controller must not acknowledge the data.