DLPU126 December   2023 DLP470TE , DLP660TE , DLP780TE , DLPC4420

 

  1.   1
  2.   Description
  3.   Getting Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
    5. 1.5 Other Items Needed for Operation
  7. 2Hardware
    1. 2.1 Power Supply Requirements
      1. 2.1.1 External Power Supply Requirements
    2. 2.2 Connections
      1. 2.2.1 DLPC4420AEVM Connections
        1. 2.2.1.1 DLPC4420AEVM Connectors
        2. 2.2.1.2 DLPC4420AEVM Test Points
      2. 2.2.2 DLP660TEEVM Connections
        1. 2.2.2.1 DLP660TEEVM Test Points
        2. 2.2.2.2 DLP660TEEVM Connectors
      3. 2.2.3 DLP470TEEVM Connections
        1. 2.2.3.1 DLP470TEEVM Test Points
        2. 2.2.3.2 DLP470TEEVM Connectors
      4. 2.2.4 DLP780TEEVM Connections
        1. 2.2.4.1 DLP780TEEVM Test Points
        2. 2.2.4.2 DLP780TEEVM Connectors
    3. 2.3 Connecting the DLP660TEEVM, DLP470TEEVM, or DLP780TEEVM to the DLPC4420AEVM
  8. 3Software
    1. 3.1 Quick Start
      1. 3.1.1 Downloading the Software
      2. 3.1.2 Powering-up the DLPC4420AEVM and Preparing for the DLPC4420AEVM to be Programmed
      3. 3.1.3 Programming the DLPC4420AEVM and Displaying a SPLASH Image
      4. 3.1.4 JTAG Flash Programming
      5. 3.1.5 Flash Device Parameters
      6. 3.1.6 Troubleshooting
  9. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  10. 5Additional Information
    1. 5.1 If You Need Assistance
    2. 5.2 Caution Labels
    3.     Trademarks
  11. 6Related Documentation from Texas Instruments

Programming the DLPC4420AEVM and Displaying a SPLASH Image

Follow these steps to download and configure the DLPC44xx GUI:

  1. The Projector Control (.projector) and Firmware binary(.img) files are located in the install directory. The same procedure applies to the DLP470TEEVM and DLP780TEEVM with the appropriate firmware.
  2. Setting up Communication Preferences:
    1. DLPC44xx GUI supports USB and I2C communication. To change these settings, please go to Edit- >Preferences->Communication.
      GUID-20231031-SS0I-TMBP-NRH1-PD8QG8J7QWTN-low.pngFigure 3-2 DeVaSys Communication Configuration
    2. For USB, please select the USB interface.
      Note: USB is the preferred method to download the firmware flash image to the projector as USB is much faster than I2C.
      GUID-20231031-SS0I-RL14-RHXM-VGXWXR0Q1ZDF-low.png Figure 3-3 USB Communication Configuration
    3. An error message can appear saying the USB driver cannot be opened. This is expected, as TI has not yet enabled communication on the board. Click OK on this error.
      GUID-86EE78ED-85B7-4985-993C-8F1190B00D40-low.gif Figure 3-4 Error Message
  3. Projector Control Configuration:
    1. Run the DLPC44xx GUI tool and select the Projector Control sub-tool.
      GUID-20231031-SS0I-WC69-WCND-NZS1ZFL1ZWDF-low.png Figure 3-5 Projector Control Menu
    2. Select Open Projector File then select Add. Navigate to the .projector file location installed in step 1.
      GUID-20231031-SS0I-8CFN-RF1H-TBHP537NCP2T-low.png Figure 3-6 Adding DLPC4420 Projector Control File
    3. Make sure the desired Projector Control file is checked, then select OK.
      Note: If the user wants to use one Projector Control file at a time, then deselect the files to hide before selecting OK.
      GUID-20231031-SS0I-TRFF-S58N-QMMXPTSNMNMJ-low.png Figure 3-7 Projector Control File for the Chosen Chipset
    4. Once this file is loaded, the user can navigate through the pages to control a DLPC4420 controller.
      GUID-20231031-SS0I-DXSQ-1R9V-0FTXL2SQW0CC-low.png Figure 3-8 DLPC4420 Projector Control Menu
  4. Flash Loader Configuration:
    1. Select the Flash Loader sub-tool, and then select the Browse button. After navigating to the installation directory, navigate to the DLPC4420_Software_Files folder and select the “Flash_DLPC4420_DLP660TE_p66_TRP_4KUHD_S610_LED.img” file and click on open.
      GUID-20231031-SS0I-TKZ3-LJSS-WHVTRFW2CFVQ-low.png Figure 3-9 Loading the Flash Image
    2. Select Complete Image Download for first time download. By default, the flash has the boot loader pre-loaded; uncheck the Skip Boot Loader Area.
      Note: Check Skip Boot Loader Area only if the bootloader needs to be upgraded.
      GUID-20231031-SS0I-3SFH-CFM8-FSZWRXDSN45L-low.png Figure 3-10 Downloading Image onto the EVM
    3. Connect DLPC4420AEVM to PC via USB. Make sure USB communication capability by clicking Reset Bus on the bootloader menu in the DLPC44xx GUI. The Status field appears as follows:
      GUID-9779AD8A-C5BD-4ABB-9006-B6D3EC2243A6-low.png Figure 3-11 Communication Between GUI and EVMs
      Note: If there is an issue with USB communication, then turn off DLPC4420AEVM and disconnect then reconnect USB cable and power on board.
    4. Select Start Download to begin. The loading process takes between 5 and 10 minutes.
    5. After the download has completed, switch SW1 to off and switch the power to the unit under test (UUT) off. Remove the jumper on J31 from the DLPC4420AEVM board.
    6. After removing the jumper, re-enable power to the DLPC4420AEVM. Switch SW1 to the On position. A Red LED appears after a few seconds. The Red LED shuts off and a green LED begins blinking. After the blinking LED appears, the DLP Texas Instruments logo is visible on the DMD for a few seconds and appear as or similar to what is seen in Figure 4-12.
      GUID-BC461EF5-E4D3-4B96-BA61-15052F199B5B-low.png Figure 3-12 Splash Image Displayed on DMD

Turn the switch back to the off position before connecting the USB cable to DLPC4420AEVM. The power supply does not have to be disconnected before connecting the USB cable. Once the USB cable is connected to the DLPC4420AEVM (and the PC), turn the switch on the DLPC4420AEVM to the on position.