SBAU407 april   2023 ADS8354

 

  1.   Abstract
  2.   Trademarks
  3. 1Overview
    1. 1.1 ADS8354EVM-PDK Features
    2. 1.2 ADS8354EVM Features
    3. 1.3 Related Documentation From Texas Instruments
  4. 2Analog Interface
    1. 2.1 Connectors for Analog Inputs
    2. 2.2 ADC Input Signal Driver
      1. 2.2.1 Input Signal Path
  5. 3Digital Interfaces
    1. 3.1 SPI for the ADC Digital I/O
  6. 4Power Supplies
    1. 4.1 ADC Input Driver Configuration
    2. 4.2 ADC Voltage Reference Configuration
  7. 5ADS8354EVM-PDK Initial Setup
    1. 5.1 Default Jumper Settings
    2. 5.2 EVM Graphical User Interface Software Installation
  8. 6ADS8354EVM-PDK Operation
    1. 6.1 EVM GUI Global Settings for ADC Control
    2. 6.2 Time Domain Display Tool
    3. 6.3 Spectral Analysis Tool
    4. 6.4 Histogram Analysis Tool
  9. 7Bill of Materials, Printed-Circuit Board Layout, and Schematics
    1. 7.1 Bill of Materials
    2. 7.2 PCB Layout
    3. 7.3 Schematics

EVM Graphical User Interface Software Installation

The following steps describe how to install the software for the ADS8354EVM graphical user interface (GUI).

  1. Download the latest version of the ADS835xEVM GUI installer from the Order & start development section of the ADS8354EVM-PDK Tool Folder, and run the GUI installer to install the EVM GUI software on your computer.
    CAUTION:

    Manually disable any antivirus software running on the computer before downloading the EVM GUI installer onto the local hard disk. Failure to disable antivirus software, depending on the antivirus settings, may cause an error message to appear or the installer.exe file may be deleted.

     

  2. Accept the license agreements (Figure 5-2) and follow the on-screen instructions to complete the installation.
    GUID-20230223-SS0I-FWPW-1FDZ-GF6FQKHWF2DB-low.svg Figure 5-2 ADS835xEVM Software Installation Prompts
  3. As a part of the ADS835xEVM GUI installation, a prompt with a Device Driver Installation Wizard (Figure 5-3) appears on the screen. Click the Next button to proceed, then click the Finish button when the installation is complete.

     

    GUID-20230223-SS0I-5C7G-L0RR-JN7NKNDK5LSQ-low.svg Figure 5-3 Device Driver Installation Wizard Prompts
    Note:

    A notice may appear on the screen stating that Windows cannot verify the publisher of this driver software. Select the Install this driver software anyway option.

    The device requires the LabVIEW™ run-time engine (see Figure 5-4) and may prompt for the installation of this software, if not already installed.

    GUID-BC43E0DA-B878-4BD3-8584-352A69B29762-low.png Figure 5-4 LabVIEW Run-Time Engine Installation

     

  4. Check the Create Desktop Shortcut box, as Figure 5-5 shows, after these installations.
    GUID-20230223-SS0I-NJ9B-ST6N-G2QWRH0H5SWH-low.svg Figure 5-5 ADS8354EVM-PDK Installation Final Step