SBOA418 july   2023 OPA2197-Q1 , OPA392

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction: Open-Loop Output Impedance (RO)
  5. 2Overview: Closed-Loop Amplifier Stability
  6. 3Example, Calculate Optimal Isolation Resistance to Drive Large Load Capacitance
  7. 4RO, RISO, and Capacitive Load Drive
  8. 5Derive Equation for Optimal Isolation Resistance
  9. 6Summary
  10. 7References

Summary

Amplifier circuits driving large capacitive loads become unstable due to the interaction between the open-loop output impedance and the load capacitance. When driving a large capacitive load, an optimal isolation resistor must be implemented to maintain closed-loop stability with minimal voltage error. For amplifiers with resistive open-loop output impedance, an equation was derived to quickly determine an optimal RISO value. The magnitude of RISO is dependent on the magnitude of the load capacitance, the gain bandwidth of the amplifier, and the open-loop output impedance. Amplifiers with low open-loop output impedance are best for driving capacitive loads.

The analysis in this document considers amplifiers with resistive output impedance over frequency. Certain amplifier architectures exhibit a complex output impedance, ZO, across the bandwidth of the amplifier. Amplifiers with complex output impedance require further analysis and additional techniques to optimize capacitive load-drive stability. The scope of this article is limited to amplifiers that exhibit a resistive output impedance similar to the OPA392 output impedance shown in Figure 1-1.