SBOU180B november 2016 – july 2023 INA260
Figure 3-3 shows the default jumper configuration for the INA260EVM and Table 3-1 explain the purpose of each jumper. Ensure that the jumpers are installed in the correct positions, based on the required test conditions.
JUMPER |
DEFAULT |
PURPOSE |
---|---|---|
J1 | IN+ | This jumper selects whether the VBUS pin on the INA260 is connected to the IN+ or IN– pin; see Section 2.2.2 for details. |
J2 | GND | This jumper sets the A0 character of the 2-character I2C device address; see Section 2.3 for details. |
J3 | GND | This jumper sets the A1 character of the 2-character I2C device address; see Section 2.3 for details. |