SPRACM9B June 2019 – November 2020 TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This build level uses the same precompiled executable of CM that is used in the previous build level. Here, CM is used as a conduit to pass information between TwinCAT and drive controller.
Here are the steps to follow:
Now the ECAT slave controller is ready to connect to ECAT master, which is the TwinCAT running on user's development computer.