SPRACM9B June 2019 – November 2020 TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The controller implemented for the open loop and closed loop plots shown in Figure 11-8 and Figure 11-9 is a dead beat controller where the output catches up to the input in just one sample cycle without any overshoots or requiring multiple cycles. From the closed loop plot, it is clear that the closed loop gain is always 0dB (unity gain) at all frequencies and therefore, magnitude based bandwidth determination is not practical. Hence, the phase plot is chosen as reference, and the frequency at which the phase lag goes beyond 90° is taken as bandwidth per the Chinese standard GBT 16439-2009 or NEMA ICS 16 (speed loop). In this test case, the PWM frequency is chosen as 10 KHz and the sampling frequency is 20 KHz and the current loop bandwidth obtained from the closed loop plot is about 5000Hz per these guidelines.