SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
There are five peripheral subscribers for the MCU event fabric. These subscribers are different peripherals that must be configured differently according to the purpose of those specific peripherals. The following subscribers are not described in this chapter, but rather in each of the corresponding peripheral chapters:
The following two subscribers are described below: