SWRU576 January   2021 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Acronyms Used in This Document
  3. Peer to Peer (P2P) Mode
    1. 2.1 P2P Device
      1. 2.1.1 Searching Phase
      2. 2.1.2 Negotiation
      3. 2.1.3 Group Formation
    2. 2.2 PSP Client
    3. 2.3 P2P GO
    4. 2.4 P2P Commands
      1. 2.4.1 P2P Commands Detailed Information
        1. 2.4.1.1 p2p_find
        2. 2.4.1.2 p2p_connect
        3. 2.4.1.3 p2p_listen
        4. 2.4.1.4 p2p_group_add
        5. 2.4.1.5 p2p_group_remove
        6. 2.4.1.6 p2p_peer
        7. 2.4.1.7 p2p_invite
      2. 2.4.2 P2P Event Details
    5. 2.5 P2P Use Cases
      1. 2.5.1 P2P Connection in PBC (Push Button Control)
      2. 2.5.2 Create Autonomous 1:2 P2P Group (Push button Control)
        1. 2.5.2.1 Assigning IP Address in P2P Mode Using DHCP Method
        2. 2.5.2.2 Create 1:2 P2P Group - Connect With PIN Code
        3. 2.5.2.3 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)
  4. Access Point (AP) and Peer-to-Peer (P2P) Multirole
    1. 3.1 Errata/Limitations
  5. Multi BSSID (mBSSID)
    1. 4.1 Setup and Configuration
    2. 4.2 User Guide and Examples
  6. Access Point (AP) Enhanced Low Power (ELP) Mode
    1. 5.1 Setup and Configuration
    2. 5.2 User Guide and Examples
    3. 5.3 Errata/Limitations
  7. WiLink8 Wake on WLAN (WoWLAN) Feature
    1. 6.1 Mode of Operation
    2. 6.2 Adding "Suspend/Resume" WoW Mode to AM335x EVM
      1. 6.2.1 Patch Description
    3. 6.3 WoWLAN (Wake on WLAN) Mode Enable Procedure
      1. 6.3.1 Commands and Expected Output
      2. 6.3.2 Rx Filter Configuration
        1. 6.3.2.1 Rx Filter Configuration Examples
    4. 6.4 WoWLAN - Magic Packet
    5. 6.5 Block Acknowledgement (BA) Filter Setting
    6. 6.6 Hardware Modification Engineering Change Order (ECO) Request for AM335x EVM
  8. WiLink8 Suspend Resume Mode
    1. 7.1 Suspend Resume Example With AM437x SDK
  9. Access Point (AP) Dynamic Frequency Selection (DFS) Master Support
    1. 8.1 Setup and Configuration
    2. 8.2 User Guide & Examples
    3. 8.3 Errata/Limitations
  10. Station Mode - Alternative Method, With iw Commands, Explained
    1. 9.1 Step 1- Check if the wlan0 Interface is Already Running
    2. 9.2 Step 2- Bringup wlan0 Interface if Not Running
    3. 9.3 Step 3 - Connect Device to Available Acces Point
  11. 10References

WiLink8 Wake on WLAN (WoWLAN) Feature

Wake-on-Wireless (WoW) is a feature to allow the system to go into a low-power state while the wireless NIC remains active and does varying things for the host, for example, staying connected to an AP or searching for networks. For more information, see kernel.org.

This section discusses how to enable "Suspend Resume" WoW Mode with a WL18xx device and an AM335x host processor. With some extra work, the hardware and software modifications outlined below can also be performed on other host processors to enable WoW.