SWRU576 January   2021 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Acronyms Used in This Document
  3. Peer to Peer (P2P) Mode
    1. 2.1 P2P Device
      1. 2.1.1 Searching Phase
      2. 2.1.2 Negotiation
      3. 2.1.3 Group Formation
    2. 2.2 PSP Client
    3. 2.3 P2P GO
    4. 2.4 P2P Commands
      1. 2.4.1 P2P Commands Detailed Information
        1. 2.4.1.1 p2p_find
        2. 2.4.1.2 p2p_connect
        3. 2.4.1.3 p2p_listen
        4. 2.4.1.4 p2p_group_add
        5. 2.4.1.5 p2p_group_remove
        6. 2.4.1.6 p2p_peer
        7. 2.4.1.7 p2p_invite
      2. 2.4.2 P2P Event Details
    5. 2.5 P2P Use Cases
      1. 2.5.1 P2P Connection in PBC (Push Button Control)
      2. 2.5.2 Create Autonomous 1:2 P2P Group (Push button Control)
        1. 2.5.2.1 Assigning IP Address in P2P Mode Using DHCP Method
        2. 2.5.2.2 Create 1:2 P2P Group - Connect With PIN Code
        3. 2.5.2.3 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)
  4. Access Point (AP) and Peer-to-Peer (P2P) Multirole
    1. 3.1 Errata/Limitations
  5. Multi BSSID (mBSSID)
    1. 4.1 Setup and Configuration
    2. 4.2 User Guide and Examples
  6. Access Point (AP) Enhanced Low Power (ELP) Mode
    1. 5.1 Setup and Configuration
    2. 5.2 User Guide and Examples
    3. 5.3 Errata/Limitations
  7. WiLink8 Wake on WLAN (WoWLAN) Feature
    1. 6.1 Mode of Operation
    2. 6.2 Adding "Suspend/Resume" WoW Mode to AM335x EVM
      1. 6.2.1 Patch Description
    3. 6.3 WoWLAN (Wake on WLAN) Mode Enable Procedure
      1. 6.3.1 Commands and Expected Output
      2. 6.3.2 Rx Filter Configuration
        1. 6.3.2.1 Rx Filter Configuration Examples
    4. 6.4 WoWLAN - Magic Packet
    5. 6.5 Block Acknowledgement (BA) Filter Setting
    6. 6.6 Hardware Modification Engineering Change Order (ECO) Request for AM335x EVM
  8. WiLink8 Suspend Resume Mode
    1. 7.1 Suspend Resume Example With AM437x SDK
  9. Access Point (AP) Dynamic Frequency Selection (DFS) Master Support
    1. 8.1 Setup and Configuration
    2. 8.2 User Guide & Examples
    3. 8.3 Errata/Limitations
  10. Station Mode - Alternative Method, With iw Commands, Explained
    1. 9.1 Step 1- Check if the wlan0 Interface is Already Running
    2. 9.2 Step 2- Bringup wlan0 Interface if Not Running
    3. 9.3 Step 3 - Connect Device to Available Acces Point
  11. 10References

P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)

The following section details the P2P connection with the PIN method. Below are the general steps:

  1. P2P Invitation Request frame is transmitted by a P2P Group Owner or a P2P Client in that P2P Group.
  2. Upon receiving the P2P Invitation Request, a P2P Device that supports the P2P Invitation Procedure signaling mechanism transmits a P2P Invitation Response frame.
  3. The decision to accept the invitation is left to the invited P2P Device

The Flow of commands shows a case where the EVM#1 is the GO and invites EVM#2.

Table 2-10 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control) Command Sequence
Step # EVM #1 EVM #2

Comments

1 Run: p2p_start.sh Run: p2p_start.sh cd /usr/share/wl18xx/ ./p2p_start.sh
2 Run: p2p_cli.sh Run: p2p_cli.sh ./p2p_cli.sh
3 p2p_group_add freq=2412
4 exit wpa_cli ( on EVM#1) type: quit
5 Reenter wpa_cli using the newly created p2p-wlan0-0 interface on EVM#1 wpa_cli -ip2p-wlan0-0
6 wps_pbc
7 wait after the remote "p2p_find"
8 p2p_find
9 p2p_invite group=p2p-wlan0-0 peer=EVM#2_MAC_ADDRESS
10 p2p_connect EVM#1_MAC_ADDRESS pbc join
11 exit wpa_cli exit wpa_cli type: quit
12 Acquire IP address for p2p-wlan0-0 Acquire IP address for p2p-wlan0-0 EVM#1: ifconfig p2p-wlan0-0 192.168.3.3 EVM#2: ifconfig p2p-wlan0-0 192.168.3.4
13 Verify connection with ping EVM#1: ping 192.168.3.4 EVM#2: ping 192.168.3.3