SWRU576 January   2021 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Acronyms Used in This Document
  3. Peer to Peer (P2P) Mode
    1. 2.1 P2P Device
      1. 2.1.1 Searching Phase
      2. 2.1.2 Negotiation
      3. 2.1.3 Group Formation
    2. 2.2 PSP Client
    3. 2.3 P2P GO
    4. 2.4 P2P Commands
      1. 2.4.1 P2P Commands Detailed Information
        1. 2.4.1.1 p2p_find
        2. 2.4.1.2 p2p_connect
        3. 2.4.1.3 p2p_listen
        4. 2.4.1.4 p2p_group_add
        5. 2.4.1.5 p2p_group_remove
        6. 2.4.1.6 p2p_peer
        7. 2.4.1.7 p2p_invite
      2. 2.4.2 P2P Event Details
    5. 2.5 P2P Use Cases
      1. 2.5.1 P2P Connection in PBC (Push Button Control)
      2. 2.5.2 Create Autonomous 1:2 P2P Group (Push button Control)
        1. 2.5.2.1 Assigning IP Address in P2P Mode Using DHCP Method
        2. 2.5.2.2 Create 1:2 P2P Group - Connect With PIN Code
        3. 2.5.2.3 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)
  4. Access Point (AP) and Peer-to-Peer (P2P) Multirole
    1. 3.1 Errata/Limitations
  5. Multi BSSID (mBSSID)
    1. 4.1 Setup and Configuration
    2. 4.2 User Guide and Examples
  6. Access Point (AP) Enhanced Low Power (ELP) Mode
    1. 5.1 Setup and Configuration
    2. 5.2 User Guide and Examples
    3. 5.3 Errata/Limitations
  7. WiLink8 Wake on WLAN (WoWLAN) Feature
    1. 6.1 Mode of Operation
    2. 6.2 Adding "Suspend/Resume" WoW Mode to AM335x EVM
      1. 6.2.1 Patch Description
    3. 6.3 WoWLAN (Wake on WLAN) Mode Enable Procedure
      1. 6.3.1 Commands and Expected Output
      2. 6.3.2 Rx Filter Configuration
        1. 6.3.2.1 Rx Filter Configuration Examples
    4. 6.4 WoWLAN - Magic Packet
    5. 6.5 Block Acknowledgement (BA) Filter Setting
    6. 6.6 Hardware Modification Engineering Change Order (ECO) Request for AM335x EVM
  8. WiLink8 Suspend Resume Mode
    1. 7.1 Suspend Resume Example With AM437x SDK
  9. Access Point (AP) Dynamic Frequency Selection (DFS) Master Support
    1. 8.1 Setup and Configuration
    2. 8.2 User Guide & Examples
    3. 8.3 Errata/Limitations
  10. Station Mode - Alternative Method, With iw Commands, Explained
    1. 9.1 Step 1- Check if the wlan0 Interface is Already Running
    2. 9.2 Step 2- Bringup wlan0 Interface if Not Running
    3. 9.3 Step 3 - Connect Device to Available Acces Point
  11. 10References

User Guide & Examples

The following are the script and flow used for operation on DFS channel:

  1. Start the AP: ap_start.sh.
  2. Wait 60 seconds for the channel availability check to be completed and AP to be enabled.
  3. If radar was detected on the AP channel:
    1. New Channel is randomly selected
    2. AP perform channel switch

Radar Simulation: There is a debug option to simulate a radar detection on a specific DFS channel: Example:

echo 60 > /sys/kernel/debug/ieee80211/phy0/wlcore/wl18xx/radar_detection

Changing Non-Occupancy-Period (NOP): To edit the 'NOP' time, load cfg80211 modules with the desired parameters: dfs_nop_time_ms - Non Occupying Period in ms, Default is 1,800,000. dfs_cac_time_ms – CAC time in ms, Default is 60,000. Example:

modprobe cfg80211.ko dfs_nop_time_ms=60000 dfs_cac_time_ms=10000
Note: This requires a driver reloading.

Enable/Disable test mode: Allows testing radar detection without switching channels.

echo 8 > /proc/sys/kernel/printk Disable: echo 0 > /sys/kernel/debug/ieee80211/phy0/wlcore/wl18xx/radar_debug_mode Enable: echo 1 > /sys/kernel/debug/ieee80211/phy0/wlcore/wl18xx/radar_debug_mode