SWRU576 January   2021 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Acronyms Used in This Document
  3. Peer to Peer (P2P) Mode
    1. 2.1 P2P Device
      1. 2.1.1 Searching Phase
      2. 2.1.2 Negotiation
      3. 2.1.3 Group Formation
    2. 2.2 PSP Client
    3. 2.3 P2P GO
    4. 2.4 P2P Commands
      1. 2.4.1 P2P Commands Detailed Information
        1. 2.4.1.1 p2p_find
        2. 2.4.1.2 p2p_connect
        3. 2.4.1.3 p2p_listen
        4. 2.4.1.4 p2p_group_add
        5. 2.4.1.5 p2p_group_remove
        6. 2.4.1.6 p2p_peer
        7. 2.4.1.7 p2p_invite
      2. 2.4.2 P2P Event Details
    5. 2.5 P2P Use Cases
      1. 2.5.1 P2P Connection in PBC (Push Button Control)
      2. 2.5.2 Create Autonomous 1:2 P2P Group (Push button Control)
        1. 2.5.2.1 Assigning IP Address in P2P Mode Using DHCP Method
        2. 2.5.2.2 Create 1:2 P2P Group - Connect With PIN Code
        3. 2.5.2.3 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)
  4. Access Point (AP) and Peer-to-Peer (P2P) Multirole
    1. 3.1 Errata/Limitations
  5. Multi BSSID (mBSSID)
    1. 4.1 Setup and Configuration
    2. 4.2 User Guide and Examples
  6. Access Point (AP) Enhanced Low Power (ELP) Mode
    1. 5.1 Setup and Configuration
    2. 5.2 User Guide and Examples
    3. 5.3 Errata/Limitations
  7. WiLink8 Wake on WLAN (WoWLAN) Feature
    1. 6.1 Mode of Operation
    2. 6.2 Adding "Suspend/Resume" WoW Mode to AM335x EVM
      1. 6.2.1 Patch Description
    3. 6.3 WoWLAN (Wake on WLAN) Mode Enable Procedure
      1. 6.3.1 Commands and Expected Output
      2. 6.3.2 Rx Filter Configuration
        1. 6.3.2.1 Rx Filter Configuration Examples
    4. 6.4 WoWLAN - Magic Packet
    5. 6.5 Block Acknowledgement (BA) Filter Setting
    6. 6.6 Hardware Modification Engineering Change Order (ECO) Request for AM335x EVM
  8. WiLink8 Suspend Resume Mode
    1. 7.1 Suspend Resume Example With AM437x SDK
  9. Access Point (AP) Dynamic Frequency Selection (DFS) Master Support
    1. 8.1 Setup and Configuration
    2. 8.2 User Guide & Examples
    3. 8.3 Errata/Limitations
  10. Station Mode - Alternative Method, With iw Commands, Explained
    1. 9.1 Step 1- Check if the wlan0 Interface is Already Running
    2. 9.2 Step 2- Bringup wlan0 Interface if Not Running
    3. 9.3 Step 3 - Connect Device to Available Acces Point
  11. 10References

Searching Phase

During a searching phase, the P2P device discovers any device that supports P2P functionality and is discovered by other P2P devices for further connection. If P2P functionality is used by some specific application, such as Miracast, only devices that support Miracast capabilities appear in the list of devices for connection. Such filtering is possible because of a service discovery function in P2P devices. The P2P device does not have a static operating channel in which it can be detected. Thus, the search phase consists of two phases: scan and listen. During the scan phase, the P2P devices scan all WLAN channels on both 2.4 GHz and 5 GHz (if 5 GHz is supported), and wait for responses from devices that support P2P functionality. During the listen phase, the P2P devices stay on specific channels called social channels. The P2P device remains in the listen state for a time period that permits detection. P2P detection during the search phase is statistical and depends on a proper combination of the scan and the listen phases. When P2P devices are detected, they appear in the P2P devices list.