SWRU576 January   2021 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Acronyms Used in This Document
  3. Peer to Peer (P2P) Mode
    1. 2.1 P2P Device
      1. 2.1.1 Searching Phase
      2. 2.1.2 Negotiation
      3. 2.1.3 Group Formation
    2. 2.2 PSP Client
    3. 2.3 P2P GO
    4. 2.4 P2P Commands
      1. 2.4.1 P2P Commands Detailed Information
        1. 2.4.1.1 p2p_find
        2. 2.4.1.2 p2p_connect
        3. 2.4.1.3 p2p_listen
        4. 2.4.1.4 p2p_group_add
        5. 2.4.1.5 p2p_group_remove
        6. 2.4.1.6 p2p_peer
        7. 2.4.1.7 p2p_invite
      2. 2.4.2 P2P Event Details
    5. 2.5 P2P Use Cases
      1. 2.5.1 P2P Connection in PBC (Push Button Control)
      2. 2.5.2 Create Autonomous 1:2 P2P Group (Push button Control)
        1. 2.5.2.1 Assigning IP Address in P2P Mode Using DHCP Method
        2. 2.5.2.2 Create 1:2 P2P Group - Connect With PIN Code
        3. 2.5.2.3 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)
  4. Access Point (AP) and Peer-to-Peer (P2P) Multirole
    1. 3.1 Errata/Limitations
  5. Multi BSSID (mBSSID)
    1. 4.1 Setup and Configuration
    2. 4.2 User Guide and Examples
  6. Access Point (AP) Enhanced Low Power (ELP) Mode
    1. 5.1 Setup and Configuration
    2. 5.2 User Guide and Examples
    3. 5.3 Errata/Limitations
  7. WiLink8 Wake on WLAN (WoWLAN) Feature
    1. 6.1 Mode of Operation
    2. 6.2 Adding "Suspend/Resume" WoW Mode to AM335x EVM
      1. 6.2.1 Patch Description
    3. 6.3 WoWLAN (Wake on WLAN) Mode Enable Procedure
      1. 6.3.1 Commands and Expected Output
      2. 6.3.2 Rx Filter Configuration
        1. 6.3.2.1 Rx Filter Configuration Examples
    4. 6.4 WoWLAN - Magic Packet
    5. 6.5 Block Acknowledgement (BA) Filter Setting
    6. 6.6 Hardware Modification Engineering Change Order (ECO) Request for AM335x EVM
  8. WiLink8 Suspend Resume Mode
    1. 7.1 Suspend Resume Example With AM437x SDK
  9. Access Point (AP) Dynamic Frequency Selection (DFS) Master Support
    1. 8.1 Setup and Configuration
    2. 8.2 User Guide & Examples
    3. 8.3 Errata/Limitations
  10. Station Mode - Alternative Method, With iw Commands, Explained
    1. 9.1 Step 1- Check if the wlan0 Interface is Already Running
    2. 9.2 Step 2- Bringup wlan0 Interface if Not Running
    3. 9.3 Step 3 - Connect Device to Available Acces Point
  11. 10References

Setup and Configuration

Operating AP on DFS channel is done with the ‘user-scripts’ provided by TI. These scripts can be used as a reference of how to operate the AP DFS Master feature, and their usage is described below:

Note: These scripts are used also for running AP on non DFS channel as well.

The configuration parameters of the hostapd are located in a configuration file ‘hostapd.conf’. These files are provided by TI and may be modified to meet the product requirements. However, there are some parameters needed to be modified in order to support AP DFS Master, as mentioned in Table 8-1, and these parameters must be set in order for the feature to function correctly.

Table 8-1 Hostapd.conf File Parameters to Support DFS
Attribute/File hostapd.conf Comments
hw_mode a DFS is operational on A band only
country_code Pick a country For example: US
channel Pick channel according to the HW mode and the country code selected Channel must be supported in the selected country
ieee802.11d 1
ieee802.11h 1
basic_rates 60 120 240 Default values are: 10 20 55 110 60 120 240. Change is required to operate on 5G band.