SLOA044A March 2000 – June 2021 TL2842 , TL2842B , TL2843 , TL2844 , TL2845 , TL3842 , TL3842B , TL3843 , TL3844 , TL3845 , TLC081 , TLC2201 , TLV2231 , TLV2361 , TLV2362 , TLV2470 , TLV2471 , TLV2770 , TLV2771 , TLV341 , TLV342 , UC1842 , UC1843 , UC1844 , UC1845 , UC2842 , UC2842A , UC2843 , UC2843A , UC2844 , UC2844A , UC2845 , UC2845A , UC3841 , UC3842 , UC3842A , UC3842M , UC3843 , UC3843A , UC3844 , UC3844A , UC3845 , UC3845A , UC3845AM , UCC1800 , UCC1801 , UCC1802 , UCC1803 , UCC1804 , UCC1805 , UCC2800 , UCC2801 , UCC2802 , UCC2802M , UCC2803 , UCC2804 , UCC2805 , UCC2813-0 , UCC2813-1 , UCC2813-2 , UCC2813-3 , UCC2813-4 , UCC2813-5 , UCC28C40 , UCC28C41 , UCC28C42 , UCC28C43 , UCC28C44 , UCC28C45 , UCC3801 , UCC3802 , UCC3803 , UCC3804 , UCC3805 , UCC3813-0 , UCC3813-1 , UCC3813-2 , UCC3813-3 , UCC3813-4 , UCC3813-5 , UCC38C40 , UCC38C41 , UCC38C42 , UCC38C43 , UCC38C44 , UCC38C45
A switch-mode power supply often switches current on the primary side of a transformer through a MOSFET and measures the primary current with a sense resistor (RSense) as shown in Figure 1-1 (a). The pulse width modulator IC (PWM) usually requires a current-sense signal (VS) in order to provide short-circuit protection or for use in current mode control, or for both protection and control. The peak value of VS depends on the PWM IC used, but it is typically 1 volt.
The value of the sense resistor RSense in Figure 1-1 (a) is chosen based on the peak value of the primary-side current (IPeak) and the required value of VS. Therefore, RSense is determined by:
The power dissipation in RSense is based on the RMS value of the primary-side current (Irms), which depends on the peak value as well as on the waveshape and the duty cycle. The power dissipated is:
As an example, let:
IPeak = 6.67 A
Irms = 4 A
VS = 1 V
These values result in an RSense of 0.15 Ω, and a power dissipation in RSense equal to 2.4 W. Typically, a 5-W-rated resistor would be used in this application.
The circuit of Figure 1-1 (b) can be used to significantly reduce the cost and power dissipation of RSense. First, let us review how the circuit of Figure 1-1 (b) operates. This op-amp circuit is configured as a typical differential amplifier. The circuit operates by multiplying the differential sense signal (VSense) by the differential gain of the op-amp circuit. If Rf = R3 and Ri = R2, this gain is:
Using the previous example, assume that the design goal is to use a lower-power sense resistor with a standard value, such as a 0.01-Ω resistor rated at 0.5 W, and to limit the dissipation of this resistor to no more than 0.25 W. From this information, the gain of the circuit can be calculated.
Based on these results, let Rf = R3 = 15 kΩ and Ri = R2 = 1 kΩ in Figure 1-1 (b).